采用FPGA控制DAC芯片AD7545,目前在调试硬件,因此FPGA没有工作,IO口输出电压在3.1V左右,AD7545的12位数据输入端口均为高电平,VIN为-5V,电路原理图如下,测得运放输出电压-13.6V左右,最大不应该是5V吗?求解答
看了你的电路图应该是没有问题,根据你的描述,貌似是AD7545没能正常工作,请确定DGND和AGND的电平一致,如果一致,那么建议你在ADI网站上申请样片试一试。