AD7150,AD7746仿真板的区别

看了一下技术参数,似乎AD7746可以单独设置成single end或者differential,AD7150没有这个功能,除了这个还有什么区别没有?

我需要测量的是一个未知DUT的小电容,究竟多小也不知道,因为现在手头上的万用表最低一档在nF不能读出数据,这个DUT由2个金属环当中夹着一块绝缘环,看上去就是一个空心的汉堡

谢谢

Parents
  • 0
    •  Analog Employees 
    on Nov 18, 2013 1:35 PM

    AD7150和AD7747的几个区别:

    1. AD7150的分辨率为12位,而AD7747的分辨率为24位。

    2. 测量电容范围不同,AD7747为17+/-4pf(当然可以根据外接电路扩展,见cn-0129),而AD7150 为10+0.5~4pf。

    3. 供电及功耗不同。AD7150供电为2.7V~3.6V,而AD7747为2.7~5.25V.

Reply
  • 0
    •  Analog Employees 
    on Nov 18, 2013 1:35 PM

    AD7150和AD7747的几个区别:

    1. AD7150的分辨率为12位,而AD7747的分辨率为24位。

    2. 测量电容范围不同,AD7747为17+/-4pf(当然可以根据外接电路扩展,见cn-0129),而AD7150 为10+0.5~4pf。

    3. 供电及功耗不同。AD7150供电为2.7V~3.6V,而AD7747为2.7~5.25V.

Children
No Data