Post Go back to editing

两个有关AD9949内部模数转换的问题

问题一:AD9949内部的12高性能位ADC是什么类型的,如逐次逼近型、Sigma-Delta型等;

问题二:AD9949中提到了很多的增益调整,我有点搞晕了,比如我的输入信号是1Vp-p,经过了1.5V的直流偏压,那么我在CDS的增益可设为0dB,在PxGA增益为0dB,VGA的增益是6-42dB,至少是6dB,为什么是至少呢?不是增益大于6dB时信号会大于2Vp-p吗?那么信号到了12ADC时,2V参考电压,岂不是超过了参考电压范围,这样ADC的分辨率还会最好吗?还有前面的1.5V直流偏压哪去了,加上这个偏压的话,最大电压值就更大了吗?

Parents Reply Children
No Data