Post Go back to editing

两个有关AD9949内部模数转换的问题

问题一:AD9949内部的12高性能位ADC是什么类型的,如逐次逼近型、Sigma-Delta型等;

问题二:AD9949中提到了很多的增益调整,我有点搞晕了,比如我的输入信号是1Vp-p,经过了1.5V的直流偏压,那么我在CDS的增益可设为0dB,在PxGA增益为0dB,VGA的增益是6-42dB,至少是6dB,为什么是至少呢?不是增益大于6dB时信号会大于2Vp-p吗?那么信号到了12ADC时,2V参考电压,岂不是超过了参考电压范围,这样ADC的分辨率还会最好吗?还有前面的1.5V直流偏压哪去了,加上这个偏压的话,最大电压值就更大了吗?

Parents
  • 1)AD9949是pipeline ADC;

    2)每个增益调整的内容是不同的,首先CDS gain是用来限制输入AD9949的模拟信号动态范围,请参考数据手册page26的Table22. 对于不同的CDS gain,所允许的输入范围是不同的。PxGA就可以分别调整不同颜色的像素增益;VGA 的6dB已经是会将1V的信号匹配到2V full-scale ADC范围上了:

    The minimum gain of 6 dB is needed to match a 1 V input signal with the ADC full-scale range of 2 V.

    ADC的full-scale range 是2V,前面所有的增益加起来与输入信号的乘积只要不超过2V full range就可以了。

    3)直流恢复,是恢复CCD信号的Reset电平的电压,而真正有效信号电压范围是Reset电平到“波谷”电压的差值(CDS电路会采集两次CCD模拟信号,然后做差)。

Reply
  • 1)AD9949是pipeline ADC;

    2)每个增益调整的内容是不同的,首先CDS gain是用来限制输入AD9949的模拟信号动态范围,请参考数据手册page26的Table22. 对于不同的CDS gain,所允许的输入范围是不同的。PxGA就可以分别调整不同颜色的像素增益;VGA 的6dB已经是会将1V的信号匹配到2V full-scale ADC范围上了:

    The minimum gain of 6 dB is needed to match a 1 V input signal with the ADC full-scale range of 2 V.

    ADC的full-scale range 是2V,前面所有的增益加起来与输入信号的乘积只要不超过2V full range就可以了。

    3)直流恢复,是恢复CCD信号的Reset电平的电压,而真正有效信号电压范围是Reset电平到“波谷”电压的差值(CDS电路会采集两次CCD模拟信号,然后做差)。

Children
No Data