Post Go back to editing

关于AD9779的问题

请教下各位,我使用FPGA出频率为30MHz的数字信号,数据速率为61.44MHz,给AD9779当输入,AD9779内部做122.88MHz的上变频,则有用信号会在152.88MHz处,但同时会在154.32MHz处有一幅度相差50dbc左右的杂散信号,请问下这有可能是哪里引起的,谢谢了!

  • 楼主要提高数据速率,现在数据速率是61.44MHz,那么在61.44MHz+/-30MHz的位置会有镜像,122.88再对镜像进行混频,就会出现楼主说的杂散。所以建议楼主换其它的参数,也就是改变一下数据速率试试。

    楼主可以这么理解,如果是ADC采样的应用,输入模拟信号频率是30MHz,而采样速率是61.44MHz,那是不是在61.44MHz+/-30MHz的位置会有镜像呢,对于DAC 的应用也可以这么理解。实际上,输出镜像的位置会分布在x*Fdataclk+y*Fdac+z*Fa,其中Fdataclk就是输出数据速率,Fdac就是DAC 的系统时钟,Fa就是模拟信号频率。

    可以参考手册34页的表格设置插值滤波器的寄存器,实现122.88M的上变频,即实现2倍内插,不用加入频偏调制,即用DC调制模式。所以插值因子设为2,滤波器模式取0x00即可。

  • This question has been closed by the EZ team and is assumed answered.