Post Go back to editing

问题: AD8403问题

最近在用AD8403这款数字电位器,但是遇到了一些问题希望得到解决。
1、定位器输出的电阻可不可以在通电的状态下用万用表来测量。
2、用万用表测量发现电阻不准,10k的测量出来却只有9.2k而且不稳地。
3、线性不是太好,每次步进的阻值相差较多

  • 不建议在芯片带电时直接用万用表去测量数字电位计的阻值。
    数字电位计的阻值是有一定的容差的,通常为+/-20%,10K得到9.2K还是比较正常的。
    另外,数字电位计的INL和DNL楼主要注意一下。如果对于10K的电阻,1LSB就是10K/256=40欧姆。楼主说的步进的阻值相差较多,是多少呢?看一下是不是在数据手册第四页所示的INL和DNL的范围之内。

  • 楼主使用什么万用表测试的?是手持式的还是精度更高的带电源插头的表,比如Agilent34401A.我们在测试AD5270(另外一款数字电位计)发现,如果用手持表测,是没问题的。但是如果用34401A测,就要注意测试时要想办法使得电阻两端点的绝对电压不能超过芯片的供电电压,否则那个值是不准的。另外AD8403的评估板中,通过测一个真正的DAC的输入输出来判断该阻值的大小。没有具体测试该评估板,不过楼主可以参考一下:
    http://www.analog.com/static/imported-files/user_guides/UG-255.pdf
    另外,如果是9.2K满量程,那么步进应该是36.您看到的某些步进应该有比34大的才对。但看这个值,应该是在spec.范围内的。

  • This question has been closed by the EZ team and is assumed answered.