Post Go back to editing

问题: 实用AD9779A的问题

请问下ADI的各位大虾,我现在用ADI的AD6655+FPGA+AD9779A做数字方面设计,发现AD9779A输出有以下问题,请分析下,给我些解决问题的方案,谢谢:

现象:FPGA

送出29.56M数据格式为I/Q两路的单音信号分别给AD9779A的两个输入口,AD9779A内部滤波器模式选择了1/8 fdac

shift的模式(等效为上搬了61.44M),结果从AD9779A的2模拟信号输出口(Q输出口)得到91M的信号(这是我想要的信号),同时在93.32Mhz处会有一个70dBc左右的的杂散信号,这个杂散信号会根据FPGA送出的数据与有用信号反向偏移,如FPGA

送出28.56M,则DAC有用信号为90M,而杂散信号为94.32M,请问下这有可能是什么引起的。

DAC的配置:参考时钟122.88MHz,输入为复数输入(即两路都配置,一路进I信号,一路进Q信号),需要的信号从I或者Q输出口直接经巴仑引出,内部做8倍内插,内部FDAC为491.52MHz,则输入至DAC的数据速率为61.44M

分析杂散频点:以现在看,杂散信号有点类似是122.88减去FPGA给DAC的频率,但杂散信号会根据DAC选择模式变化,如搬移122.88M,杂散点同样向上搬移,与有用信号的间距与前面情况一致

Parents Reply Children
No Data