AD4111,ODR设置为31250,使用开路检测要求的通道配置,用了8个通道,从手册的表6来看,它说能够实现6200sps per channel,但是实际fpga跑出来,连续转换模式下,adc的输出大约是6200hz,但是要被每一个通道平分,为什么
这芯片是单Σ-Δ adc核的,输出频率需要平分吗,问了FAE,又说可以每通道6200hz输出
AD4111,ODR设置为31250,使用开路检测要求的通道配置,用了8个通道,从手册的表6来看,它说能够实现6200sps per channel,但是实际fpga跑出来,连续转换模式下,adc的输出大约是6200hz,但是要被每一个通道平分,为什么
这芯片是单Σ-Δ adc核的,输出频率需要平分吗,问了FAE,又说可以每通道6200hz输出
你的测量是对的。6.21kSPS是整颗芯片的通道扫描率(手册原文是maximum channel scan rate of 6.21 kSPS (161 µs) for fully settled data),表6那列"SPS per Channel"指的是切换通道后单次已建立转换的速率,不是每个使能通道能同时拿到的速率;8个通道槽轮流平分,6211/8≈776SPS,与你实测的775一致。反过来算也能确认:8路各6.21kSPS需要49.7kSPS,已经超过sinc5输出固定的31.25kSPS,单个Σ-Δ核做不到。
还要注意开路检测本身的开销:手册要求每个电压输入在做开路检测时占用两个通道槽,所以这8个槽实际只对应4路物理输入,每路每秒约776次开路比较。
提速有两条路:一是改用sinc3,最快档的建立时间是97µs、整体约10309SPS,8个槽下每槽约1289SPS(约1.66倍),代价是最高速率下噪声明显大于sinc5+sinc1;二是不连续做开路检测,平时每路只占一个槽,定期切到配对配置做一次诊断。