I am using the AD9857 in IQ mode to transmit an audio IQ file that has been modulated in SSB USB mode. In baseband signal simulation, I got very normal results (as shown in Figure 1).
However, the actual transmitted spectrum shows a lot of spurs and images within ±400 kHz of the carrier, with almost no sideband suppression. I also tried FM modulation, but it was almost impossible to demodulate.
(When the carrier frequency is set to 10 MHz, no significant spurs are observed (see Figure 2). However, when the carrier frequency is set to 35 MHz, obvious spurs appear within ±400 kHz of the carrier (see Figure 3). Regardless of the carrier frequency, the unwanted opposite sideband — which never appears in the IQ baseband signal — is always present in the output. Is this an image?)
Could you please advise on how to resolve this issue?

Figure 1

Figure 2

Figure 3
Additional configuration details for the AD9857:
-
Clock source: Single-ended TCXO, 50 MHz
-
PLL multiplier: ×4 (system clock = 200 MHz)
-
CIC interpolation factor: ×63
-
Single-tone mode has been successfully verified and is working properly.Additionally, with only a reconstruction filter (cutoff frequency 60 MHz) in place,
-
the measured second harmonic is less than -50 dBc (carrier at 10 MHz, second harmonic at 20 MHz).
-
14-bit parallel data port, TxENABLE and PDCLK signals — the transmit timing has been verified with an oscilloscope and is confirmed to be correct.