Post Go back to editing

ad7606的问题

Category: Hardware
Product Number: AD7606B

我手里有一批使用ad7606的通信板,有一部分无法与7606通信,通过mcu的代码发现busy一直为高,还有一部分通信成功但是采集到的数据有几十mV的偏差

因为使用的mcu和代码都是一样的怀疑是硬件上的问题,但是通信板也是一样的不知道哪些部品可能出问题。

我用万用表量了电压,通信成功但是有误差的板子上AGND = 0V REFOUT = 2.48V AVCC = 4.97V REFCAPA REFCAPB = 4.5V

没误差的反而 AGND = 3V REFOUT = 4V

而无法通信的AGND在2V-3V之间变化 REFOUT = 4V  AVCC = 4.9V REFCAPA REFCAPB = 4.9V busy一直为高

原理图如下

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.