Post Go back to editing

AD712-8 REFIN检测问题

Thread Summary

用户询问当外部基准电压在0.5~0.7V之间时,AD7124-8的基准电压检测功能是否可用。最终答案指出,虽然REF_DET_ERR位会在基准电压低于0.7V时置位,但这并不意味着芯片无法工作,因此在0.5~0.7V区间内仍可使用该功能,但不推荐。建议避免将基准电压设置在0.5~0.7V之间以确保检测功能的准确性。
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7124-8

根据数据手册 Rev.F中内容,AD7124-8具有基准电压检测功能。将ERROR_EN寄存器中的REF_DET_ERR_EN位设置为1,可以使能此特性。 如果选定的REFINx(+)与REFINx(–)引脚之间的电压降至0.7 V以下,或者REFINx(+)或REFINx(–)输入开路,AD7124-8就会检测到它不再具有有效的基准电压。 此时,错误寄存器中的REF_DET_ERR位设置为1。 状态寄存器中的ERR位也会置1。

但是根据table 3,外部基准电压的输入范围为0.5V~AVDD。

当我的外部基准电压在0.5~0.7V之间时,是否不能使用基准电压检测功能?有什么其他方法可以检测基准电压?

  • ADC转换输入电压时,其依靠的主要是基准电压为尺度,AD7124的REF_DET_ERR位,也只是标识reference基准电压太低了。但是即使基准电压低于0.7,也仅仅是将这个过低的状态标识出来,不意味着在芯片在基准为0.5-0.7的区间内无法工作或会停止工作。

    所以,您说的当您在外部基准电压在0.5~0.7V之间时,是能使用基准电压检测功能(但不推荐),因为使用了REF_DET_ERR就基本会置位,但置位并不导致芯片无法工作。

    有什么其他方法可以检测基准电压?其实最好的方式就是不让ADC的基准电压工作在0.5-0.7V之间。