Post Go back to editing

AD7793 内部的温度传感器的转化公式

Category: Software
Product Number: AD7793
Software Version: AD7793 内部的温度传感器的转化公式

采用AD7793进行水质传感器设计,现在要用到AD7793内部的温度传感器监控芯片的问题,现在能够读出ADC的转化值,但是规格书中没有具体的温度传感器的计算公式,现在不知道如何把ADC的转化值通过计算公式转变成温度值?请问有没有这一方面的参考资料?有没有类似于AD7124-4里面的内部温度传感器

  • 793进行水质传感器设计,现在要用到AD7793内部的温度传感器监控芯片的问题,现在能够读出ADC的转化值,但是规格书中没有具体的温度传
  • 您好,我也在用AD7793做一款室外的变送器,现在进行环境温度测试的时候发现AD7793的激励电流温漂为200ppm/℃,导致测量值随环境温度变化较大。如果AD7793含有测量本体温度的功能,就可以对环境温度变化的影响做一部分补偿,请问您提到的这个温度传感器是可以测AD7793本体的温度吗?

  • 关于AD7793芯片内部温度传感器的使用公式,见如下描述。
    In bipolar mode:
    Temperature (degC) = ((conversion – 800000)/sensitivity(in codes)) – 273.15 => Temp (degC) = ((conversion – 800000)/5807) -273.15

    In Unipolar mode:
    Temperature (degC) = (conversion/sensitivity(in codes)) – 273.15 => Temp (degC) = ((conversion/11615) -273.15

    In this formula the conversion is in codes as well. The 5807 and 11615 are the 0.81mv/degC in codes for bipolar mode and unipolar mode respectively.
  • 你好,孟工,是您在中国技术支持中心来信的吧,您邮件中的提问,我似乎已经多次回复过您的邮件,但从您继续发来的邮件内容看,似乎您没收到过我之前的回复,请检查您的邮件是否拦截了ADI公司的回复邮件。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.