Post Go back to editing

AD7794接入6路称重传感器后,读取的ID和状态寄存器都为0XFF。断开称重传感器后读出ID为0x88,这个是什么原因造成的?

Category: Hardware
Product Number: AD7794

硬件设计如下:

  • 看现象描述确实是比较异常的,我想问下你电路现在除了读取ID异常,其它工作的功能正常吗?ADC采样,offse和full scale值复位后读取值这些,正不正常?

  • 读取的数据全部为1,DOUT/DRY引脚一直为高。我想问一下,AD7794可以配置六路称重传感器吗?

  • AD7794可以配置成6路称重传感器,就是不知道你电路是怎么设计的,那如果你读取数据也全为1,那就不是id寄存器的问题,而是整个芯片压根就不在正常的工作,芯片可能坏了,或者电路设计不对。按理,一般称重传感器都会设计成比例式测量,但是比例式测量供电是个问题,您该不会是称重传感器直接用的refin1的输出进行供电的吧?那芯片的内部reference根本承载不了6路称重传感器的供电电流。总之,你要么把设计电路图发出来我看看,要么自己再检查下电路设计细节,或者可以更换芯片看看。

  • 感谢您的回复。称重传感器接口电路图我放在图2中,其中称重传感器供电与芯片供电以及基准电压是使用同一电源,这个电源是由外部电源供电,使用的REF5050芯片。这样供电源是否会存在问题?

  • 绝对有问题,您用的REF输出电流才±10mA,基本是无法用于供电的,用于称重的比例式测量时,问题很大,你如果称重传感器阻抗是350,5/350一路就需要14mA,不知道你是否额外做过什么设计优化你现在的供电,否则您现在的设计是应该是会有问题的。比例式测量其实可以放宽对adc ref的要求,你因此可以采用的ldo做电源和reference,这样供电压力会小些。或者是lt6658这种高输出电流能力的电压基准。

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.