Post Go back to editing

AD7192的DOUT引脚固定输出宽约98us脉冲,复位读取寄存器均无响应

各位老师您好,我在嘉立创打样+SMT贴了2片AD7192BRUZ,实验发现读ID、读数据寄存器都为0,而AD7192的DOUT脚固定输出宽约98微秒的高电平。

请问各位老师,这是因为2片AD7192都是坏片呢,还是其他什么原因。兄弟初学使用AD7192,非常感谢各位的指点。多谢了

图1:SPI_SCK与SPI_MOSI的波形,其中MOSI波形的1字节值为0x58,应该是正确的通信寄存器指令(读DATA)是吗。

图2:SPI_SCK与SPI_MISO的波形。

图3:原理图局部

再次感谢

Parents
  • 首先是图片看不到,其次是芯片一般没那么容易坏,在这块板子之前,你是有成功调试过ad7192通信的经验和代码了吗?

    还是你打好和贴片的板子也是你第一次调试和ad7192的通信?如果您的第一次调,大概率是你程序的问题。

  • 谢谢你的回复。问题已经自己解决了。产品目前使用其他厂家(**5530)的24位ADC,这次设计AD7192样板,贴片两块样板,目的是做一下对比和选择。所以对芯片正品来源比较看重。发贴后,有ADI代理联系我,也索要了我们的营业执照,但表示申请样片挺麻烦的。既然麻烦,就放弃吧,继续使用原方案。

Reply
  • 谢谢你的回复。问题已经自己解决了。产品目前使用其他厂家(**5530)的24位ADC,这次设计AD7192样板,贴片两块样板,目的是做一下对比和选择。所以对芯片正品来源比较看重。发贴后,有ADI代理联系我,也索要了我们的营业执照,但表示申请样片挺麻烦的。既然麻烦,就放弃吧,继续使用原方案。

Children