Post Go back to editing

AD7192 2路差分采集,通道之间有影响

Category: Hardware
Product Number: AD7192

AD7192  2路差分12通道  34通道,使用通道序列器连续采集,采集过程中通道之间相互影响的情况。比如差分通道12 采集计算的电压是1V   此时差分通道34输入4V   就会发现通道1的电压上升了0.5mv左右。采样率200hz  相当于单通道100hz,使能斩波,sinc4滤波 使能缓冲。这种通道间有影响的的情况是什么原因导致的?尝试关闭通道34   只采集12通道,此时在通道34施加电压,测试发现12通道的数据不改变。

Parents
  • 对于单核ADC发现的通道间串扰问题,基本都是由于外部电路的不良设计导致的 。通道间串扰隔离度通常只在多核adc比如AD4858 ad7767这些adc中有标crosstalk参数。单核adc像ad7192,一次只有一个通道切入,另一个通道其实是通信芯片内部的开关mos断开了,所以不可能是芯片内部导致的通道间干扰问题。我觉得主要是你每个通道间耦合太强了,毕竟按你说的1V 0.5mv.只有66db左右的抑制。明显小了。

    还有你说的采样率200hz,单通道不会是100hz,因为sigma delta有通道建立时间要求,当然这对你现在遇到的问题来说是题外话。你需要解决你外部电路的通道间耦合问题。

    ...

    ...

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.