Post Go back to editing

AD7124-8热电偶应用时,内部偏置导致的测量误差

Thread Summary

The user asked about the impact of 3.3nA absolute input current on the CN0384 application, leading to a 6.6uV differential input and 0.165°C error. The final answer clarified that the actual differential input current is ±1.5nA, reducing the error by half, and suggested using on-chip or software calibration to correct the offset error. The user also provided a helpful diagram explaining the absolute and differential input currents.
AI Generated Content

1、AIN有3.3nA的绝对输入电流,在CN0384的应用中,会导致3.3nA*2K= 6.6uV的差分输入,6.6uV/40uv/°C = 0.165°C的误差。不知是否理解正确?

2、即使用外部偏置,该电流也是存在,如果热电偶线路长(比如100欧姆),也会导致0.33uV的误差?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.