LT2320,LVDS模式下的时序是不是比CMOS模式下的时序更加宽松,可以给转换和采样时间留出更多裕量
以LTC2320-14为例,在CMOS模式,SDR单倍速率模式下,SCK最短周期为9.1ns,取整数10ns,则最大频率为100MHz,每个通道需要16个周期读取,读取时间共计160ns,DDR模式的读取时间相同。
而在LVDS模式下,SDR单倍速率模式下,SCK最短周期3.3ns,最大频率300MHz,每两个通道需要32个周期读取,最短读取时间共计105.6ns,即使以250MHz周期4ns的sck频率计算,读取时间也是128ns,比CMOS模式所需时间短的多,如果要以1.5M最大速率采样,那每周期只有667ns,CMOS模式下,去掉读取时间还剩507ns,去掉最大转换时间450ns,只剩50ns给采样时间,我想问的是,对于奈氏定理的信号频率,30~50ns的采样时间是足够的吗,能达到标称的信噪比吗?
如果是LTC2320-16,数据手册上的转换时间变成最低450ns了,那转换时间加上20ns的裕量,cnv采样时间就会被压缩到最低30ns了,这个时间到数据手册的极限了,还能保证最大速率和500kHz输入信号的稳定运行吗?我觉得这个时序裕量好像很小,有没有解答