Post Go back to editing

模拟输入电压

Category: Hardware
Product Number: AD7124-4

AD7124采集外部电压时超过模拟输入口的VSS-50mV---VDD+50mV电压范围时,只要没有超过模拟输入口10mA电流就会把接口的电压钳在输入口安全电压范围内还是直接烧掉pin?

Parents
  • 超过50mV但是低于300mV通常不会带来损坏,但是超过300mV,加上10mA的电流,有芯片片损坏和性能下降的风险。任一超过ABSOLUTE MAXIMUM RATINGS的电气特性施加到芯片上都是有风险的,只是超过VSS-50mV---VDD+50mV一般是不会导致输入电流变大的,因为ADC输入阻抗一般较大,不可能有mA级别的电流输入,一般是超过300mV,使得内部保护二极管导通了才会有大电流输入,这时如果电压超的不大,且电流也不大,则通常能保证芯片起码不坏。您是遇到什么实际问题了吗?

Reply
  • 超过50mV但是低于300mV通常不会带来损坏,但是超过300mV,加上10mA的电流,有芯片片损坏和性能下降的风险。任一超过ABSOLUTE MAXIMUM RATINGS的电气特性施加到芯片上都是有风险的,只是超过VSS-50mV---VDD+50mV一般是不会导致输入电流变大的,因为ADC输入阻抗一般较大,不可能有mA级别的电流输入,一般是超过300mV,使得内部保护二极管导通了才会有大电流输入,这时如果电压超的不大,且电流也不大,则通常能保证芯片起码不坏。您是遇到什么实际问题了吗?

Children
No Data