Category: Hardware
Product Number: LTC1864
您好,请教一个问题,就是LTC1864如果是5V供电,那么他的三个管脚SCK,SDO,CONV的电平是1.8V?3.3V?还是5V?
如果接FPGA的3.3V的IO,是不是还需要中间加一级电平转换芯片?是否有相应的案列可以参考,谢谢

您好,请教一个问题,就是LTC1864如果是5V供电,那么他的三个管脚SCK,SDO,CONV的电平是1.8V?3.3V?还是5V?
如果接FPGA的3.3V的IO,是不是还需要中间加一级电平转换芯片?是否有相应的案列可以参考,谢谢

5V供电时,这些输出引脚的高电平输出是5V.
ADG3304,是个适合您应用的电平转换芯片。

5V供电时,这些输出引脚的高电平输出是5V.
ADG3304,是个适合您应用的电平转换芯片。

Dear Frank,
LTC1864的SCK,CONV是输入信号,电平标准是3.3V吧?如下,谢谢

您圈出开的手册中这部分参数是什么意思?高电平最低2.4 低电平最高0.8,这两个参数不作为电平标准必须是3.3V的判断依据。
Dear Frank,
LTC1864的SCK,CONV是输入信号,我想问的就是SCK,CONV这两个输入信号电平标准是3.3V吧?不是5V的电平标准吧?
3.3V和5V的电平输入下都可以工作。