在使用AD7705测量频率在0.8-2Hz的光电转换信号时,发现在SPI以50Hz频率访问AD7705时,读取的电压总会在读取几个采样点后产生瞬间变化,类似一个锯齿波,锯齿波频率在2Hz,起初认为是电源纹波,准备使用有源滤波的方式的去除,后来改变了SPI读取ADC的频率到10Hz,发现该锯齿波消失。
下两张图分别为50Hz读取频率和10Hz的读取频率下的数据,横坐标为第几次读取,纵坐标为转换后的电压值。


ADC的外围电路如下,AD8062为其前级电路,AD8062的输出OUT1_连接AD7705的通道2,基准电压源为AD1582



个人推断是在较高频率的ADC采样下,AD8062无法提供足够的电荷,但每次采样的间隔有20ms,应该不会发生该种情况。
想问下在ADC读取频率50Hz下该波纹发生的原因,应该如何消除该波纹?