工程的配置如下所示:
JESD204B模式:采用模式11;
JESD204B的Line数量:使用了8个line(前4个为I、后4个为Q);
JESD204B数据率:数据率为2.6GSPS(I/Q);
全链路内插值:通道旁路(内插1)、主通道内插4、主通道NCO设置为50MHz
ADC速率:10.4GSPS
参考时钟:325MHz
SYSREF:20.3125MHz
锁相环配置:使能PLL,N=8,M=2
在当前配置下,输入了1个5MHz的正弦波(格式已按照手册格式排好),应该输出一个55MHz的正弦波,但实际无输出,此时204B已经建链,且FPGA已观测到数据输出到204B端口;当修改为NCO Only模式时,则能够输出50MHz的正弦波,不知在参数配置方面是不是哪里配错了,下面是在正常输入下的参数配置步骤,希望得到大家的指点:
/* * AD9174 config sequence. */ //config Power-Up and Required Register-----------------------------reg_addr[0]-reg_addr[5]; USpi_SigleReg_Write(BaseAddress,0x0000,0x0081); USpi_SigleReg_Write(BaseAddress,0x0000,0x003C); USpi_SigleReg_Write(BaseAddress,0x0091,0x0000); USpi_SigleReg_Write(BaseAddress,0x0206,0x0001); USpi_SigleReg_Write(BaseAddress,0x0705,0x0001); USpi_SigleReg_Write(BaseAddress,0x0090,0x0000); //DAC PLL Configuration---------------------------------------------reg_addr[6]-reg_addr[21]; USpi_SigleReg_Write(BaseAddress,0x0095,0x0000); USpi_SigleReg_Write(BaseAddress,0x0790,0x0000); USpi_SigleReg_Write(BaseAddress,0x0791,0x0000); USpi_SigleReg_Write(BaseAddress,0x0796,0x00E5); USpi_SigleReg_Write(BaseAddress,0x07A0,0x00BC); USpi_SigleReg_Write(BaseAddress,0x0794,0x0008); USpi_SigleReg_Write(BaseAddress,0x0797,0x0010); USpi_SigleReg_Write(BaseAddress,0x0797,0x0020); USpi_SigleReg_Write(BaseAddress,0x0798,0x0010); USpi_SigleReg_Write(BaseAddress,0x07A2,0x007F); usleep(100000); //wait for 100ms USpi_SigleReg_Write(BaseAddress,0x0799,0x00C8); USpi_SigleReg_Write(BaseAddress,0x0793,0x0019); USpi_SigleReg_Write(BaseAddress,0x0094,0x0000); USpi_SigleReg_Write(BaseAddress,0x0792,0x0002); USpi_SigleReg_Write(BaseAddress,0x0792,0x0000); usleep(100000); //wait for 100ms reg_rd_buffer = USpi_Reg_Read(BaseAddress,0x07B5); //read AD7414 Register reg_rd_buffer = reg_rd_buffer & 0x0001; if(reg_rd_buffer == 0x0001) xil_printf("AD9714 PLL is locked\r\n"); else xil_printf("AD9714 PLL is not lock\r\n"); usleep(1000); //Delay Lock Loop (DLL) Configuration-------------------------------reg_addr[22]-reg_addr[30]; USpi_SigleReg_Write(BaseAddress,0x00C0,0x0000); USpi_SigleReg_Write(BaseAddress,0x00C0,0x0000); USpi_SigleReg_Write(BaseAddress,0x00DB,0x0000); USpi_SigleReg_Write(BaseAddress,0x00DB,0x0001); USpi_SigleReg_Write(BaseAddress,0x00DB,0x0000); USpi_SigleReg_Write(BaseAddress,0x00C1,0x0068); USpi_SigleReg_Write(BaseAddress,0x00C1,0x0069); USpi_SigleReg_Write(BaseAddress,0x00C7,0x0001); reg_rd_buffer = USpi_Reg_Read(BaseAddress,0x00C3); //read AD7414 Register reg_rd_buffer = reg_rd_buffer & 0x0001; if(reg_rd_buffer == 0x0001) xil_printf("AD9714 DLL is locked\r\n"); else xil_printf("AD9714 DLL is not lock\r\n"); usleep(1000); //Calibration-------------------------------------------------------reg_addr[31]-reg_addr[36]; USpi_SigleReg_Write(BaseAddress,0x0050,0x002A); USpi_SigleReg_Write(BaseAddress,0x0061,0x0068); USpi_SigleReg_Write(BaseAddress,0x0051,0x0082); USpi_SigleReg_Write(BaseAddress,0x0051,0x0083); usleep(10000); //wait for 100ms reg_rd_buffer = USpi_Reg_Read(BaseAddress,0x0052); //read AD7414 Register xil_printf("AD9714 register 0x052 is:0x%x \r\n",reg_rd_buffer); USpi_SigleReg_Write(BaseAddress,0x0081,0x0003); usleep(1000); //JESD204B Mode Setup-----------------------------------------------reg_addr[37]-reg_addr[46]; USpi_SigleReg_Write(BaseAddress,0x0100,0x0000); USpi_SigleReg_Write(BaseAddress,0x0110,0x000B); //single-link mode reg_rd_buffer = USpi_Reg_Read(BaseAddress,0x0110); //read AD7414 Register xil_printf("AD9714 register 0x110 is:0x%x \r\n",reg_rd_buffer); USpi_SigleReg_Write(BaseAddress,0x0111,0x0041); //Interp_Mode reg_rd_buffer = USpi_Reg_Read(BaseAddress,0x0110); //read AD7414 Register xil_printf("AD9714 register 0x110 is:0x%x \r\n",reg_rd_buffer); USpi_SigleReg_Write(BaseAddress,0x0084,0x0000); USpi_SigleReg_Write(BaseAddress,0x0312,0x0010); USpi_SigleReg_Write(BaseAddress,0x0300,0x0001); USpi_SigleReg_Write(BaseAddress,0x0475,0x0009); USpi_SigleReg_Write(BaseAddress,0x0453,0x0007); USpi_SigleReg_Write(BaseAddress,0x0458,0x002F); USpi_SigleReg_Write(BaseAddress,0x0475,0x0001); //Main DAC Datapath Setup: PA Protect and Main NCOs-----------------reg_addr[47]-reg_addr[74]; USpi_SigleReg_Write(BaseAddress,0x0008,0x00C0); //0x00C1. USpi_SigleReg_Write(BaseAddress,0x0112,0x0008); //complex mode 3B 0x0079 //0x0008 USpi_SigleReg_Write(BaseAddress,0x0114,0x0013); USpi_SigleReg_Write(BaseAddress,0x0115,0x003B); USpi_SigleReg_Write(BaseAddress,0x0116,0x00B1); USpi_SigleReg_Write(BaseAddress,0x0117,0x0013); USpi_SigleReg_Write(BaseAddress,0x0118,0x003B); USpi_SigleReg_Write(BaseAddress,0x0119,0x0001); USpi_SigleReg_Write(BaseAddress,0x011C,0x0000); USpi_SigleReg_Write(BaseAddress,0x011D,0x0000); USpi_SigleReg_Write(BaseAddress,0x0113,0x0001); //JESD204B SERDES Required Interface Setup--------------------------reg_addr[75]-reg_addr[114]; USpi_SigleReg_Write(BaseAddress,0x0240,0x00AA); USpi_SigleReg_Write(BaseAddress,0x0241,0x00AA); USpi_SigleReg_Write(BaseAddress,0x0242,0x0055); USpi_SigleReg_Write(BaseAddress,0x0243,0x0055); USpi_SigleReg_Write(BaseAddress,0x0244,0x001F); USpi_SigleReg_Write(BaseAddress,0x0245,0x001F); USpi_SigleReg_Write(BaseAddress,0x0246,0x001F); USpi_SigleReg_Write(BaseAddress,0x0247,0x001F); USpi_SigleReg_Write(BaseAddress,0x0248,0x001F); USpi_SigleReg_Write(BaseAddress,0x0249,0x001F); USpi_SigleReg_Write(BaseAddress,0x024A,0x001F); USpi_SigleReg_Write(BaseAddress,0x024B,0x001F); USpi_SigleReg_Write(BaseAddress,0x0201,0x0000); USpi_SigleReg_Write(BaseAddress,0x0203,0x0000); USpi_SigleReg_Write(BaseAddress,0x0253,0x0001); USpi_SigleReg_Write(BaseAddress,0x0254,0x0001); USpi_SigleReg_Write(BaseAddress,0x0210,0x0016); USpi_SigleReg_Write(BaseAddress,0x0216,0x0005); USpi_SigleReg_Write(BaseAddress,0x0212,0x00FF); USpi_SigleReg_Write(BaseAddress,0x0212,0x0000); USpi_SigleReg_Write(BaseAddress,0x0210,0x0087); USpi_SigleReg_Write(BaseAddress,0x0216,0x0011); USpi_SigleReg_Write(BaseAddress,0x0213,0x0001); USpi_SigleReg_Write(BaseAddress,0x0213,0x0000); USpi_SigleReg_Write(BaseAddress,0x0200,0x0000); usleep(1000000); //wait for 100ms USpi_SigleReg_Write(BaseAddress,0x0210,0x0086); USpi_SigleReg_Write(BaseAddress,0x0216,0x0040); USpi_SigleReg_Write(BaseAddress,0x0213,0x0001); USpi_SigleReg_Write(BaseAddress,0x0213,0x0000); USpi_SigleReg_Write(BaseAddress,0x0210,0x0086); USpi_SigleReg_Write(BaseAddress,0x0216,0x0000); USpi_SigleReg_Write(BaseAddress,0x0213,0x0001); USpi_SigleReg_Write(BaseAddress,0x0213,0x0000); USpi_SigleReg_Write(BaseAddress,0x0210,0x0087); USpi_SigleReg_Write(BaseAddress,0x0216,0x0001); USpi_SigleReg_Write(BaseAddress,0x0213,0x0001); USpi_SigleReg_Write(BaseAddress,0x0213,0x0000); USpi_SigleReg_Write(BaseAddress,0x0280,0x0005); USpi_SigleReg_Write(BaseAddress,0x0280,0x0001); usleep(100000); //wait for 100ms reg_rd_buffer = USpi_Reg_Read(BaseAddress,0x0281); //read AD7414 Register xil_printf("AD9714 register 0x281 is:0x%x \r\n",reg_rd_buffer); //Transport Layer Setup, Synchronization, and Enable Links----------reg_addr[115]-reg_addr[125]; USpi_SigleReg_Write(BaseAddress,0x0308,0x0008); USpi_SigleReg_Write(BaseAddress,0x0309,0x001A); USpi_SigleReg_Write(BaseAddress,0x030A,0x002C); USpi_SigleReg_Write(BaseAddress,0x030B,0x003E); USpi_SigleReg_Write(BaseAddress,0x0306,0x000C); USpi_SigleReg_Write(BaseAddress,0x0307,0x000C); USpi_SigleReg_Write(BaseAddress,0x0304,0x000C); //LMFCDel USpi_SigleReg_Write(BaseAddress,0x0305,0x000C); //LMFCVar USpi_SigleReg_Write(BaseAddress,0x003B,0x00F1); USpi_SigleReg_Write(BaseAddress,0x003A,0x0002); usleep(100000); //wait for 100ms USpi_SigleReg_Write(BaseAddress,0x0300,0x0001); //Cleanup Registers-------------------------------------------------reg_addr[126]-reg_addr[127]; //USpi_SigleReg_Write(BaseAddress,0x0085,0x0013); //USpi_SigleReg_Write(BaseAddress,0x01DE,0x0000); USpi_SigleReg_Write(BaseAddress,0x0008,0x00C0); USpi_SigleReg_Write(BaseAddress,0x0596,0x000C); |