Post Go back to editing

EVAL-AD5941BATZ can't work correctly

I use EVAL-AD5941BATZ to calculate the EIS of Lithium iron phosphate battery. But some problems have occurred.  I connect F+ and S+ to the positive pole of the battery and connect F- and S- to the negative pole of the battery. The first problem is that Analog  Devices SensorPal will flash back when drag Battery Impedance tool into the work area. The second problem is that the EIS figure is not correct, it should be a curve. Please help me, thanks!

  • Hi there, I was wondering if you’ve ever used the AD5941BATZ daughter board to measure simple resistors, like a 1 kΩ through-hole resistor? Right now, when I measure using the 4-wire EIS method, the impedance curves I get are similar to what you showed in your photos—just messy, random-looking lines. Do you have any ideas on how to fix this issue?