Post Go back to editing

AD7134供电配置问题

当我把IOVDD设置成1.8V、CLKVDD设置成1.8V后,AD7134的DOUT,DCLK,ODR及其配置接口SPI它们的电平范围是不是(1.8V~0V)? 我计划用3.3V供电的MCU+FPGA和AD7134通信。MCU负责和AD7134进行SPI配置、FPGA对AD7134进行读操作。那么这些数据IO在通信时是否要进行电平转换将1.8V转3.3V。

另外,我想对采集数据的频率精确控制,采样时间范围(65536us~1us),实现这个需求我该怎么做了? 是不是要将AD7134配置成从模式,根据DataRate=ODR*IFRatio这个公式来计算出ODR的频率,然后我FPGA生成ODR的相同的频率信号给到AD7134的ODR引脚。是这样操作的吗

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.