Post Go back to editing

AD5934在扫频的起始频率附近电阻测量不准

Thread Summary

The user is experiencing inaccurate and fluctuating resistance measurements with the AD5934 at specific frequencies (50 kHz, 63 kHz, 83 kHz) during a frequency sweep. The issue persists even after adding delays and setting the number of settling cycles to 15. The final answer suggests checking for interference using an oscilloscope to verify the signal at the RFB pin and the outputs of the op-amps, as well as ensuring the correct calculation of Frequency Codes for the AD5934.
AI Generated Content

使用AD5934扫频测量电阻,但是在起始频率附近电阻测量不准确,有较大波动。下图是连续扫频的结果,起始频率50kHz,增量2Hz,增量数300。设置其他起始频率也是一样的结果。

但是使用官方的评估板却没有这个问题。请问是什么原因?

1.AD5934的程序是参考这个的:ad5933/User at master · edaworld/ad5933 (github.com)

这是扫频部分的代码

2.这是自己画的原理图和PCB

  • From the provided brief description it is quite difficult to diagnose the issue. First thing to try would be adding a delay after calling the AD5933_Set_Mode_Freq_Start()  function. It takes some time for the C1R1R2 circuit to transition to the Vdd/2 DC level after the AD5933 comes out of Standby Mode. Adding 6-10 millisecond delay might help.

  • Thanks for your answer. But i add  a delay after calling the AD5933_Set_Mode_Freq_Start、Init_AD5933、AD5933_Set_Mode_Freq_Start_UP  function.And try different delay time.The problem still exists.

    Could it be the cause of PCB layout?

  • PCB layout is not the likely cause of it. If adding the delay did not help, we can try to debug a bit more systematically. Can you please post the following information:

    1. Is your chip the AD5933 or AD5934?
    2. What is the MCLK frequency?
    3. What is the Number of Settling Cycles? The code you linked in your post does not seem to write anything into  registers 0x8A and 0x8B. This number should not be 0, please see the datasheet, p. 15 under FREQUENCY SWEEP COMMAND SEQUENCE, paragraph 3.
    4. Was the graph you posted collected with a resistor connected to J1 or some different impedance?
    5. Is RFB1 value 100Ω?

    Can you also post a text file with the raw "real" and "img" data which you are collecting and printing? Can you get and post this data when nothing is connected to J1 and then when a resistor of 100Ω is connected to J1? It can be done through uploading via Insert->Image/video/file.

  • 1. my chip is AD5934

    2. MCLK is 16MHz

    3.  the Number of Settling Cycles ,I set it  15.

    4.  Yes, J1 is pin header. I use it to  connecte resistor.

    5. RFB1 is 1000Ω, and the resistor connected by J1 also 1000Ω.

    6. I print  the raw "real" and "img" data. There's nothing wrong with drawing.

    ①I've been changing the starting frequency around 50k.But yesterday, I realized that the problem wasn't at the starting frequency.

    I set the starting frequency to 50K, 49K, 48K, and found that the problem kept happening at 50K

    ② So I started to see if there were other frequencies that had the same problem.

    The same problem occurs around 63K and 83K

    When the frequency is below 45K, the result is completely wrong

  • Sorry, the frequency below 45K is a drawing error, the symbol was not considered when the imaginary data was converted to int

  • calibration factor:4.88e-7
    
    start:49k    add:10   num:200     RFB:1000Ω     J1:connect   1000Ω
    1 Real:  0x7 0xef Img: 0x0 0xf0 1001.8567823321512
    2 Real:  0x7 0xed Img: 0x0 0xef 1002.8882404525632
    3 Real:  0x7 0xf5 Img: 0x0 0xe9 999.3395986737224
    4 Real:  0x7 0xf0 Img: 0x0 0xed 1001.5417070470622
    5 Real:  0x7 0xe9 Img: 0x0 0xef 1004.8420646539487
    6 Real:  0x7 0xee Img: 0x0 0xf3 1002.1697575901594
    7 Real:  0x7 0xeb Img: 0x0 0xf5 1003.5144961269511
    8 Real:  0x7 0xee Img: 0x0 0xf4 1002.1113819940739
    9 Real:  0x7 0xe5 Img: 0x0 0xf5 1006.4506711684356
    10 Real:  0x7 0xe9 Img: 0x0 0xf3 1004.6091665902647
    11 Real:  0x7 0xee Img: 0x0 0xf2 1002.2279035907484
    12 Real:  0x7 0xec Img: 0x0 0xf3 1003.1441084040279
    13 Real:  0x7 0xed Img: 0x0 0xf6 1002.4806265424493
    14 Real:  0x7 0xee Img: 0x0 0xf7 1001.9348788621776
    15 Real:  0x7 0xec Img: 0x0 0xf8 1002.8490783307927
    16 Real:  0x7 0xea Img: 0x0 0xfa 1003.7044804222376
    17 Real:  0x7 0xea Img: 0x0 0xf8 1003.8244500252264
    18 Real:  0x7 0xee Img: 0x0 0xf1 1002.2858198735732
    19 Real:  0x7 0xe4 Img: 0x0 0xf2 1007.1193955814293
    20 Real:  0x7 0xea Img: 0x0 0xf7 1003.8840894773707
    21 Real:  0x7 0xea Img: 0x0 0xf9 1003.7645802981383
    22 Real:  0x7 0xe8 Img: 0x0 0xf9 1004.7416618629062
    23 Real:  0x7 0xf0 Img: 0x0 0xf9 1000.8446192641413
    24 Real:  0x7 0xee Img: 0x0 0xfd 1001.5756902255804
    25 Real:  0x7 0xee Img: 0x0 0xf8 1001.8755861156612
    26 Real:  0x7 0xef Img: 0x0 0xff 1000.9687023878292
    27 Real:  0x7 0xec Img: 0x0 0xff 1002.4263955448483
    28 Real:  0x7 0xe9 Img: 0x0 0xff 1003.8883068107194
    29 Real:  0x7 0xed Img: 0x0 0xfe 1002.0010116751675
    30 Real:  0x7 0xee Img: 0x1 0x0 1001.3930115023387
    31 Real:  0x7 0xf0 Img: 0x1 0x6 1000.0523646931587
    32 Real:  0x7 0xe8 Img: 0x1 0x1 1004.2530058432823
    33 Real:  0x7 0xe8 Img: 0x1 0x3 1004.1285415406825
    34 Real:  0x7 0xea Img: 0x1 0x9 1002.7754515486937
    35 Real:  0x7 0xea Img: 0x1 0x2 1003.2154113398078
    36 Real:  0x7 0xe9 Img: 0x1 0x9 1003.2623136336651
    37 Real:  0x7 0xe9 Img: 0x1 0x7 1003.3893436422875
    38 Real:  0x7 0xec Img: 0x1 0x9 1001.803131496524
    39 Real:  0x7 0xef Img: 0x1 0x4 1000.6612661581044
    40 Real:  0x7 0xe4 Img: 0x1 0x7 1005.8316312463403
    41 Real:  0x7 0xee Img: 0x1 0x9 1000.8326791455657
    42 Real:  0x7 0xe7 Img: 0x1 0xc 1004.0446266241889
    43 Real:  0x7 0xea Img: 0x1 0x9 1002.7754515486937
    44 Real:  0x7 0xee Img: 0x1 0x7 1000.958788372842
    45 Real:  0x7 0xea Img: 0x1 0xa 1002.7116868059289
    46 Real:  0x7 0xf1 Img: 0x1 0xb 999.2540265250834
    47 Real:  0x7 0xe6 Img: 0x1 0xd 1004.4677914471159
    48 Real:  0x7 0xec Img: 0x1 0x9 1001.803131496524
    49 Real:  0x7 0xeb Img: 0x1 0xd 1002.0330045286013
    50 Real:  0x7 0xe9 Img: 0x1 0xf 1002.8757465165916
    51 Real:  0x7 0xe9 Img: 0x1 0xf 1002.8757465165916
    52 Real:  0x7 0xe7 Img: 0x1 0x11 1003.7186914423673
    53 Real:  0x7 0xe7 Img: 0x1 0x13 1003.586720789359
    54 Real:  0x7 0xe7 Img: 0x1 0x14 1003.5203938896632
    55 Real:  0x7 0xea Img: 0x1 0x14 1002.0615250862734
    56 Real:  0x7 0xe1 Img: 0x1 0x17 1006.2486873927089
    57 Real:  0x7 0xeb Img: 0x1 0x13 1001.6421110012716
    58 Real:  0x7 0xe8 Img: 0x1 0x15 1002.9671792844433
    59 Real:  0x7 0xe6 Img: 0x1 0x11 1004.2062056956862
    60 Real:  0x7 0xe7 Img: 0x1 0x17 1003.3200485654021
    61 Real:  0x7 0xe7 Img: 0x1 0x19 1003.185349226433
    62 Real:  0x7 0xe4 Img: 0x1 0x17 1004.7822543128117
    63 Real:  0x7 0xe3 Img: 0x1 0x17 1005.2705947402962
    64 Real:  0x7 0xe4 Img: 0x1 0x14 1004.9834770201816
    65 Real:  0x7 0xe5 Img: 0x1 0x1c 1003.9549477326518
    66 Real:  0x7 0xe6 Img: 0x1 0x16 1003.874088585043
    67 Real:  0x7 0xe4 Img: 0x1 0x1d 1004.3736549508861
    68 Real:  0x7 0xe6 Img: 0x1 0x19 1003.6720863699717
    69 Real:  0x7 0xe5 Img: 0x1 0x1a 1004.0914041836155
    70 Real:  0x7 0xe6 Img: 0x1 0x18 1003.7396477767794
    71 Real:  0x7 0xea Img: 0x1 0x1b 1001.5929224547109
    72 Real:  0x7 0xe8 Img: 0x1 0x1b 1002.563669815222
    73 Real:  0x7 0xe3 Img: 0x1 0x27 1004.1612209999915
    74 Real:  0x7 0xe6 Img: 0x1 0x18 1003.7396477767794
    75 Real:  0x7 0xeb Img: 0x1 0x1f 1000.8359029354668
    76 Real:  0x7 0xe9 Img: 0x1 0x1e 1001.8735499860762
    77 Real:  0x7 0xe6 Img: 0x1 0x1a 1003.6042978163365
    78 Real:  0x7 0xe6 Img: 0x1 0x20 1003.1928043785464
    79 Real:  0x7 0xe8 Img: 0x1 0x1f 1002.290137017231
    80 Real:  0x7 0xe7 Img: 0x1 0x19 1003.185349226433
    81 Real:  0x7 0xe5 Img: 0x1 0x25 1003.3296720231166
    82 Real:  0x7 0xe6 Img: 0x1 0x29 1002.5603092821638
    83 Real:  0x7 0xe5 Img: 0x1 0x27 1003.1882350720507
    84 Real:  0x7 0xe3 Img: 0x1 0x21 1004.5840503347118
    85 Real:  0x7 0xe5 Img: 0x1 0x29 1003.045896373531
    86 Real:  0x7 0xe6 Img: 0x1 0x2a 1002.4889059425756
    87 Real:  0x7 0xe5 Img: 0x1 0x2c 1002.8307001437587
    88 Real:  0x7 0xe2 Img: 0x1 0x2b 1004.3615880833207
    89 Real:  0x7 0xe2 Img: 0x1 0x2a 1004.4336337357497
    90 Real:  0x7 0xe9 Img: 0x1 0x2c 1000.8923840122355
    91 Real:  0x7 0xe3 Img: 0x1 0x2a 1003.9467524732704
    92 Real:  0x7 0xe2 Img: 0x1 0x30 1003.9979761372962
    93 Real:  0x7 0xd9 Img: 0x1 0x45 1006.7859606879972
    94 Real:  0x7 0xce Img: 0x1 0x22 1014.8553750385149
    95 Real:  0x7 0xd3 Img: 0x1 0x7 1014.2243099780495
    96 Real:  0x7 0xee Img: 0x0 0xd3 1003.9159015319608
    97 Real:  0x8 0x2a Img: 0x0 0xac 977.0454681015641
    98 Real:  0x8 0x39 Img: 0x1 0x18 964.8642166822132
    99 Real:  0x8 0x4c Img: 0x0 0xfb 957.9896283035772
    100 Real:  0x7 0xb7 Img: 0x1 0xed 1006.5468504101384
    101 Real:  0x7 0x96 Img: 0x1 0xf1 1022.1194694476433
    102 Real:  0x7 0x28 Img: 0x2 0x6 1076.217021639801
    103 Real:  0x7 0xb2 Img: 0x0 0xc6 1034.8513961245383
    104 Real:  0x7 0x92 Img: 0x1 0x26 1045.2791298109375
    105 Real:  0x8 0x1e Img: 0x0 0xa7 982.8410165902657
    106 Real:  0x8 0x18 Img: 0x0 0xcd 984.0604205381178
    107 Real:  0x8 0x17 Img: 0x0 0xff 981.927177443488
    108 Real:  0x7 0xfb Img: 0x1 0x36 991.551875797629
    109 Real:  0x7 0xee Img: 0x1 0x2e 998.3371711902747
    110 Real:  0x7 0xe5 Img: 0x1 0x3e 1001.4971991020578
    111 Real:  0x7 0xe4 Img: 0x1 0x37 1002.5089453398076
    112 Real:  0x7 0xe7 Img: 0x1 0x39 1000.9075507501367
    113 Real:  0x7 0xe6 Img: 0x1 0x3c 1001.1653713117258
    114 Real:  0x7 0xe7 Img: 0x1 0x38 1000.9822002552753
    115 Real:  0x7 0xdf Img: 0x1 0x3b 1004.6362169723709
    116 Real:  0x7 0xe2 Img: 0x1 0x3b 1003.1782549618226
    117 Real:  0x7 0xe1 Img: 0x1 0x3c 1003.5878042780105
    118 Real:  0x7 0xe3 Img: 0x1 0x3c 1002.617442940421
    119 Real:  0x7 0xe1 Img: 0x1 0x3d 1003.5116074647856
    120 Real:  0x7 0xe1 Img: 0x1 0x3f 1003.358544057826
    121 Real:  0x7 0xe2 Img: 0x1 0x40 1002.7967091663993
    122 Real:  0x7 0xdd Img: 0x1 0x3d 1005.4574622297341
    123 Real:  0x7 0xe0 Img: 0x1 0x41 1003.6899087317968
    124 Real:  0x7 0xe0 Img: 0x1 0x41 1003.6899087317968
    125 Real:  0x7 0xdf Img: 0x1 0x43 1004.0203964899297
    126 Real:  0x7 0xe1 Img: 0x1 0x43 1003.0497425687907
    127 Real:  0x7 0xdc Img: 0x1 0x43 1005.4798594324113
    128 Real:  0x7 0xde Img: 0x1 0x45 1004.3500042996264
    129 Real:  0x7 0xdf Img: 0x1 0x44 1003.9424138877877
    130 Real:  0x7 0xe1 Img: 0x1 0x45 1002.8940070420451
    131 Real:  0x7 0xe0 Img: 0x1 0x44 1003.4569683042407
    132 Real:  0x7 0xde Img: 0x1 0x46 1004.2714623395635
    133 Real:  0x7 0xde Img: 0x1 0x47 1004.1926975916188
    134 Real:  0x7 0xe0 Img: 0x1 0x47 1003.2220253674445
    135 Real:  0x7 0xe0 Img: 0x1 0x49 1003.0642863945801
    136 Real:  0x7 0xe1 Img: 0x1 0x50 1002.0216209523965
    137 Real:  0x7 0xe9 Img: 0x1 0x4f 998.2487758637632
    138 Real:  0x7 0xdf Img: 0x1 0x4b 1003.3903061750048
    139 Real:  0x7 0xe4 Img: 0x1 0x4b 1000.9716885946497
    140 Real:  0x7 0xe0 Img: 0x1 0x53 1002.2623164033862
    141 Real:  0x7 0xe0 Img: 0x1 0x4d 1002.746149478338
    142 Real:  0x7 0xdd Img: 0x1 0x4e 1004.1203420294748
    143 Real:  0x7 0xde Img: 0x1 0x4f 1003.5545788889307
    144 Real:  0x7 0xdc Img: 0x1 0x4c 1004.7669107548804
    145 Real:  0x7 0xd7 Img: 0x1 0x59 1006.1341544927103
    146 Real:  0x7 0xde Img: 0x1 0x4f 1003.5545788889307
    147 Real:  0x7 0xdc Img: 0x1 0x52 1004.2815957506284
    148 Real:  0x7 0xde Img: 0x1 0x4c 1003.795537753118
    149 Real:  0x7 0xdd Img: 0x1 0x52 1003.7963809923518
    150 Real:  0x7 0xdb Img: 0x1 0x53 1004.6854929263594
    151 Real:  0x7 0xde Img: 0x1 0x53 1003.2302028915569
    152 Real:  0x7 0xe2 Img: 0x1 0x53 1001.2962693627753
    153 Real:  0x7 0xde Img: 0x1 0x53 1003.2302028915569
    154 Real:  0x7 0xdb Img: 0x1 0x52 1004.767273193025
    155 Real:  0x7 0xdb Img: 0x1 0x56 1004.4388235521878
    156 Real:  0x7 0xd6 Img: 0x1 0x52 1007.2026235413255
    157 Real:  0x7 0xda Img: 0x1 0x59 1004.6754680639253
    158 Real:  0x7 0xdd Img: 0x1 0x56 1003.4688822501523
    159 Real:  0x7 0xde Img: 0x1 0x59 1002.7370231285998
    160 Real:  0x7 0xd7 Img: 0x1 0x56 1006.3842604381151
    161 Real:  0x7 0xde Img: 0x1 0x5a 1002.6540568269884
    162 Real:  0x7 0xd9 Img: 0x1 0x59 1005.161233625139
    163 Real:  0x7 0xd8 Img: 0x1 0x5c 1005.395726339343
    164 Real:  0x7 0xdc Img: 0x1 0x5e 1003.2870903209863
    165 Real:  0x7 0xd6 Img: 0x1 0x5e 1006.1994237461583
    166 Real:  0x7 0xda Img: 0x1 0x56 1004.924487510924
    167 Real:  0x7 0xd8 Img: 0x1 0x5b 1005.4798594324113
    168 Real:  0x7 0xe1 Img: 0x1 0x59 1001.2880194766664
    169 Real:  0x7 0xd8 Img: 0x1 0x60 1005.0569866824164
    170 Real:  0x7 0xdb Img: 0x1 0x61 1003.5173848140623
    171 Real:  0x7 0xdc Img: 0x1 0x63 1002.8633731748417
    172 Real:  0x7 0xde Img: 0x1 0x60 1002.1516564681723
    173 Real:  0x7 0xd7 Img: 0x1 0x63 1005.286082385066
    174 Real:  0x7 0xdc Img: 0x1 0x62 1002.9485542878899
    175 Real:  0x7 0xd2 Img: 0x1 0x65 1007.5468271107997
    176 Real:  0x7 0xda Img: 0x1 0x69 1003.3139137556416
    177 Real:  0x7 0xdb Img: 0x1 0x62 1003.4322993612767
    178 Real:  0x7 0xdc Img: 0x1 0x65 1002.6923556429371
    179 Real:  0x7 0xd9 Img: 0x1 0x6b 1003.6233205710257
    180 Real:  0x7 0xd6 Img: 0x1 0x6c 1004.9887962569833
    181 Real:  0x7 0xd7 Img: 0x1 0x6c 1004.5040048404944
    182 Real:  0x7 0xd8 Img: 0x1 0x67 1004.4557211863149
    183 Real:  0x7 0xd9 Img: 0x1 0x62 1004.4011690353096
    184 Real:  0x7 0xdc Img: 0x1 0x6a 1002.2609973800813
    185 Real:  0x7 0xd3 Img: 0x1 0x6c 1006.4459357816387
    186 Real:  0x7 0xd7 Img: 0x1 0x67 1004.9406844153867
    187 Real:  0x7 0xd2 Img: 0x1 0x6f 1006.6660197537393
    188 Real:  0x7 0xd6 Img: 0x1 0x6c 1004.9887962569833
    189 Real:  0x7 0xd5 Img: 0x1 0x6d 1005.3858012377374
    190 Real:  0x7 0xd7 Img: 0x1 0x6b 1004.5917782127017
    191 Real:  0x7 0xda Img: 0x1 0x62 1003.9165040621764
    192 Real:  0x7 0xd5 Img: 0x1 0x6d 1005.3858012377374
    193 Real:  0x7 0xd8 Img: 0x1 0x6d 1003.9318086934004
    194 Real:  0x7 0xd2 Img: 0x1 0x6c 1006.9325728686302
    195 Real:  0x7 0xd6 Img: 0x1 0x6d 1004.9006770658514
    196 Real:  0x7 0xd2 Img: 0x1 0x6d 1006.843941431783
    197 Real:  0x7 0xd8 Img: 0x1 0x73 1003.4000519747788
    198 Real:  0x7 0xd7 Img: 0x1 0x72 1003.9727851674318
    199 Real:  0x7 0xda Img: 0x1 0x73 1002.4345536280708
    200 Real:  0x7 0xd5 Img: 0x1 0x6f 1005.2086513186207
    
    
    
    start:49k    add:10   num:200     RFB:1000Ω     J1:connect   1200Ω
    1 Real:  0x7 0x38 Img: 0x0 0x6d 1106.8039047354348
    2 Real:  0x7 0x35 Img: 0x0 0x6c 1108.6325456433635
    3 Real:  0x7 0x3b Img: 0x0 0x67 1105.2207314921752
    4 Real:  0x7 0x35 Img: 0x0 0x6c 1108.6325456433635
    5 Real:  0x7 0x3b Img: 0x0 0x6e 1104.9810691126681
    6 Real:  0x7 0x36 Img: 0x0 0x6e 1107.9634003276783
    7 Real:  0x7 0x34 Img: 0x0 0x6c 1109.2317016539073
    8 Real:  0x7 0x35 Img: 0x0 0x6f 1108.5259395495673
    9 Real:  0x7 0x34 Img: 0x0 0x73 1108.9780503080399
    10 Real:  0x7 0x35 Img: 0x0 0x6c 1108.6325456433635
    11 Real:  0x7 0x36 Img: 0x0 0x70 1107.8914830295962
    12 Real:  0x7 0x34 Img: 0x0 0x71 1109.0521290576712
    13 Real:  0x7 0x34 Img: 0x0 0x70 1109.088686542314
    14 Real:  0x7 0x35 Img: 0x0 0x79 1108.1497377433986
    15 Real:  0x7 0x36 Img: 0x0 0x73 1107.7812046512845
    16 Real:  0x7 0x35 Img: 0x0 0x72 1108.4164447636892
    17 Real:  0x7 0x37 Img: 0x0 0x73 1107.183748180096
    18 Real:  0x7 0x34 Img: 0x0 0x7a 1108.7086653098024
    19 Real:  0x7 0x32 Img: 0x0 0x6c 1110.4319553029832
    20 Real:  0x7 0x37 Img: 0x0 0x72 1107.220767872515
    21 Real:  0x7 0x34 Img: 0x0 0x71 1109.0521290576712
    22 Real:  0x7 0x34 Img: 0x0 0x76 1108.8645241945435
    23 Real:  0x7 0x38 Img: 0x0 0x74 1106.5496556638118
    24 Real:  0x7 0x37 Img: 0x0 0x77 1107.0324748461694
    25 Real:  0x7 0x37 Img: 0x0 0x76 1107.070772167681
    26 Real:  0x7 0x32 Img: 0x0 0x78 1109.9860458028177
    27 Real:  0x7 0x37 Img: 0x0 0x78 1106.9938583651829
    28 Real:  0x7 0x32 Img: 0x0 0x7f 1109.7045326155703
    29 Real:  0x7 0x37 Img: 0x0 0x7b 1106.876094976926
    30 Real:  0x7 0x33 Img: 0x0 0x78 1109.3863177021387
    31 Real:  0x7 0x33 Img: 0x0 0x81 1109.0220733893789
    32 Real:  0x7 0x35 Img: 0x0 0x82 1107.7837952486448
    33 Real:  0x7 0x33 Img: 0x0 0x83 1108.9376056772664
    34 Real:  0x7 0x35 Img: 0x0 0x78 1108.1887995013608
    35 Real:  0x7 0x34 Img: 0x0 0x7f 1108.5066336682676
    36 Real:  0x7 0x35 Img: 0x0 0x85 1107.656068061965
    37 Real:  0x7 0x35 Img: 0x0 0x7d 1107.9902919236704
    38 Real:  0x7 0x36 Img: 0x0 0x80 1107.2700793433175
    39 Real:  0x7 0x33 Img: 0x0 0x82 1108.9799995586447
    40 Real:  0x7 0x35 Img: 0x0 0x81 1107.8257330718798
    41 Real:  0x7 0x3b Img: 0x0 0x82 1104.2105777800605
    42 Real:  0x7 0x37 Img: 0x0 0x85 1106.4628475488184
    43 Real:  0x7 0x35 Img: 0x0 0x84 1107.6989626330371
    44 Real:  0x7 0x3a Img: 0x0 0x81 1104.8461166955556
    45 Real:  0x7 0x35 Img: 0x0 0x86 1107.6128547975957
    46 Real:  0x7 0x38 Img: 0x0 0x82 1105.9943075984681
    47 Real:  0x7 0x36 Img: 0x0 0x83 1107.1444693354458
    48 Real:  0x7 0x37 Img: 0x0 0x80 1106.6734490366532
    49 Real:  0x7 0x34 Img: 0x0 0x87 1108.1667558438528
    50 Real:  0x7 0x33 Img: 0x0 0x88 1108.7208394185689
    51 Real:  0x7 0x33 Img: 0x0 0x88 1108.7208394185689
    52 Real:  0x7 0x32 Img: 0x0 0x89 1109.2751046796034
    53 Real:  0x7 0x34 Img: 0x0 0x8c 1107.9439618390118
    54 Real:  0x7 0x33 Img: 0x0 0x8b 1108.5869462744945
    55 Real:  0x7 0x38 Img: 0x0 0x88 1105.7372345435151
    56 Real:  0x7 0x32 Img: 0x0 0x8c 1109.1400356030151
    57 Real:  0x7 0x35 Img: 0x0 0x8f 1107.209613076505
    58 Real:  0x7 0x33 Img: 0x0 0x8e 1108.450181920491
    59 Real:  0x7 0x2d Img: 0x0 0x8c 1112.1415158095167
    60 Real:  0x7 0x31 Img: 0x0 0x8e 1109.647246740885
    61 Real:  0x7 0x32 Img: 0x0 0x8d 1109.0943735870676
    62 Real:  0x7 0x33 Img: 0x0 0x8b 1108.5869462744945
    63 Real:  0x7 0x2f Img: 0x0 0x8f 1110.8003660707961
    64 Real:  0x7 0x33 Img: 0x0 0x8d 1108.49608886493
    65 Real:  0x7 0x31 Img: 0x0 0x90 1109.5541761133165
    66 Real:  0x7 0x33 Img: 0x0 0x8f 1108.4039563090048
    67 Real:  0x7 0x34 Img: 0x0 0x93 1107.618681010159
    68 Real:  0x7 0x33 Img: 0x0 0x91 1108.3105495678888
    69 Real:  0x7 0x34 Img: 0x0 0x90 1107.7599948189484
    70 Real:  0x7 0x30 Img: 0x0 0x91 1110.106434047306
    71 Real:  0x7 0x35 Img: 0x0 0x95 1106.9264911679518
    72 Real:  0x7 0x2f Img: 0x0 0x92 1110.658864720453
    73 Real:  0x7 0x33 Img: 0x0 0x8a 1108.631896502548
    74 Real:  0x7 0x36 Img: 0x0 0x98 1106.1851343250887
    75 Real:  0x7 0x32 Img: 0x0 0x9c 1108.3711963950432
    76 Real:  0x7 0x38 Img: 0x0 0x92 1105.2834455749066
    77 Real:  0x7 0x39 Img: 0x0 0x9b 1104.2546769946814
    78 Real:  0x7 0x35 Img: 0x0 0x98 1106.7806518265859
    79 Real:  0x7 0x35 Img: 0x0 0x95 1106.9264911679518
    80 Real:  0x7 0x33 Img: 0x0 0x91 1108.3105495678888
    81 Real:  0x7 0x34 Img: 0x0 0x9c 1107.1776055335683
    82 Real:  0x7 0x2f Img: 0x0 0x9b 1110.217082411289
    83 Real:  0x7 0x33 Img: 0x0 0x9b 1107.8244376238122
    84 Real:  0x7 0x2f Img: 0x0 0x9c 1110.1663984208926
    85 Real:  0x7 0x2e Img: 0x0 0x9c 1110.7660874239787
    86 Real:  0x7 0x31 Img: 0x0 0x9b 1109.0194740950337
    87 Real:  0x7 0x30 Img: 0x0 0xa1 1109.3095706361144
    88 Real:  0x7 0x2f Img: 0x0 0xa2 1109.8556015507593
    89 Real:  0x7 0x32 Img: 0x0 0x9a 1108.4717558518419
    90 Real:  0x7 0x2d Img: 0x0 0x9e 1111.263765520564
    91 Real:  0x7 0x2b Img: 0x0 0x9e 1112.4660435651303
    92 Real:  0x7 0x2d Img: 0x0 0xa9 1110.6763250532053
    93 Real:  0x7 0x2a Img: 0x0 0x9b 1113.222409457735
    94 Real:  0x7 0x25 Img: 0x0 0x8b 1117.0240315493668
    95 Real:  0x7 0x26 Img: 0x0 0x6c 1117.6882853218426
    96 Real:  0x7 0x3c Img: 0x0 0x3f 1105.6932794722295
    97 Real:  0x7 0x6c Img: 0x0 0x53 1077.355899159025
    98 Real:  0x7 0x6d Img: 0x0 0xe2 1070.2791933280428
    99 Real:  0x7 0x7a Img: 0x0 0xd9 1063.6811041976234
    100 Real:  0x7 0x79 Img: 0x0 0xef 1062.7928274943108
    101 Real:  0x6 0xc9 Img: 0x1 0x20 1163.691929138497
    102 Real:  0x6 0xd6 Img: 0x0 0x87 1167.3479311223991
    103 Real:  0x6 0xd2 Img: 0x1 0x1a 1158.4855880690225
    104 Real:  0x7 0x5 Img: 0x0 0x37 1139.6602142437528
    105 Real:  0x7 0xb Img: 0x0 0x5c 1134.9230458535876
    106 Real:  0x7 0x5d Img: 0x0 0x5e 1085.6156819417442
    107 Real:  0x7 0x56 Img: 0x0 0x8f 1087.8670051458537
    108 Real:  0x7 0x3f Img: 0x0 0xbc 1098.9143640437342
    109 Real:  0x7 0x34 Img: 0x0 0xc3 1104.9714280142819
    110 Real:  0x7 0x34 Img: 0x0 0xb6 1105.7597776392302
    111 Real:  0x7 0x35 Img: 0x0 0xab 1105.7910182082042
    112 Real:  0x7 0x32 Img: 0x0 0xaa 1107.63179032459
    113 Real:  0x7 0x34 Img: 0x0 0xb0 1106.1058260901361
    114 Real:  0x7 0x32 Img: 0x0 0xb2 1107.1814850879016
    115 Real:  0x7 0x31 Img: 0x0 0xb0 1107.8919689102945
    116 Real:  0x7 0x2f Img: 0x0 0xae 1109.1996809647007
    117 Real:  0x7 0x31 Img: 0x0 0xb2 1107.7773187893215
    118 Real:  0x7 0x33 Img: 0x0 0xb1 1106.6435863376514
    119 Real:  0x7 0x2f Img: 0x0 0xb3 1108.9129187603821
    120 Real:  0x7 0x30 Img: 0x0 0xb3 1108.315900358075
    121 Real:  0x7 0x30 Img: 0x0 0xb5 1108.1991734424394
    122 Real:  0x7 0x2c Img: 0x0 0xb3 1110.7078210067607
    123 Real:  0x7 0x2d Img: 0x0 0xb7 1109.873024026736
    124 Real:  0x7 0x30 Img: 0x0 0xb4 1108.2576944106718
    125 Real:  0x7 0x31 Img: 0x0 0xb4 1107.661409378428
    126 Real:  0x7 0x32 Img: 0x0 0xb9 1106.7709635471015
    127 Real:  0x7 0x2b Img: 0x0 0xb5 1111.1897329723881
    128 Real:  0x7 0x2e Img: 0x0 0xb8 1109.2154471503918
    129 Real:  0x7 0x2f Img: 0x0 0xb5 1108.7960031305652
    130 Real:  0x7 0x30 Img: 0x0 0xba 1107.9018486231487
    131 Real:  0x7 0x31 Img: 0x0 0xba 1107.306137473803
    132 Real:  0x7 0x36 Img: 0x0 0xb9 1104.3966321557325
    133 Real:  0x7 0x2e Img: 0x0 0xbc 1108.973664531759
    134 Real:  0x7 0x2e Img: 0x0 0xbb 1109.0345827490407
    135 Real:  0x7 0x2f Img: 0x0 0xbe 1108.2542898898498
    136 Real:  0x7 0x36 Img: 0x0 0xc2 1103.8498041744192
    137 Real:  0x7 0x3a Img: 0x0 0xbc 1101.8540854128232
    138 Real:  0x7 0x2f Img: 0x0 0xc0 1108.130451510669
    139 Real:  0x7 0x2d Img: 0x0 0xbb 1109.632113033963
    140 Real:  0x7 0x32 Img: 0x0 0xba 1106.7110633353993
    141 Real:  0x7 0x2c Img: 0x0 0xbd 1110.1077375173259
    142 Real:  0x7 0x31 Img: 0x0 0xbe 1107.0630154271573
    143 Real:  0x7 0x2b Img: 0x0 0xbe 1110.6445054377073
    144 Real:  0x7 0x30 Img: 0x0 0xc5 1107.220121208468
    145 Real:  0x7 0x36 Img: 0x0 0xb9 1104.3966321557325
    146 Real:  0x7 0x2e Img: 0x0 0xc0 1108.726845459951
    147 Real:  0x7 0x30 Img: 0x0 0xc0 1107.5346953363107
    148 Real:  0x7 0x2b Img: 0x0 0xc3 1110.3305354044162
    149 Real:  0x7 0x2d Img: 0x0 0xc2 1109.1983806907358
    150 Real:  0x7 0x2e Img: 0x0 0xc7 1108.2828239872183
    151 Real:  0x7 0x2f Img: 0x0 0xc5 1107.8153696145848
    152 Real:  0x7 0x27 Img: 0x0 0xc9 1112.3393128154412
    153 Real:  0x7 0x2e Img: 0x0 0xc5 1108.4112547052864
    154 Real:  0x7 0x2d Img: 0x0 0xc6 1108.943615242084
    155 Real:  0x7 0x2c Img: 0x0 0xc8 1109.4111988775267
    156 Real:  0x7 0x2b Img: 0x0 0xce 1109.612098437086
    157 Real:  0x7 0x2b Img: 0x0 0xc9 1109.9433735826044
    158 Real:  0x7 0x2a Img: 0x0 0xc7 1110.671919097169
    159 Real:  0x7 0x30 Img: 0x0 0xcb 1106.8323269477758
    160 Real:  0x7 0x28 Img: 0x0 0xc9 1111.739364630975
    161 Real:  0x7 0x2b Img: 0x0 0xd1 1109.4095726057794
    162 Real:  0x7 0x29 Img: 0x0 0xcc 1110.941594914941
    163 Real:  0x7 0x2c Img: 0x0 0xcd 1109.0820246868661
    164 Real:  0x7 0x28 Img: 0x0 0xcb 1111.607156163292
    165 Real:  0x7 0x2b Img: 0x0 0xcf 1109.5449028757969
    166 Real:  0x7 0x2f Img: 0x0 0xce 1107.2285279294563
    167 Real:  0x7 0x27 Img: 0x0 0xcf 1111.938257034488
    168 Real:  0x7 0x25 Img: 0x0 0xcb 1113.408289869144
    169 Real:  0x7 0x29 Img: 0x0 0xd0 1110.672571828088
    170 Real:  0x7 0x2b Img: 0x0 0xd0 1109.4773942072243
    171 Real:  0x7 0x27 Img: 0x0 0xd1 1111.8020492354387
    172 Real:  0x7 0x30 Img: 0x0 0xd0 1106.5006017276294
    173 Real:  0x7 0x2c Img: 0x0 0xd0 1108.8807632753812
    174 Real:  0x7 0x2d Img: 0x0 0xcf 1108.3520607595751
    175 Real:  0x7 0x25 Img: 0x0 0xdc 1112.2280287732897
    176 Real:  0x7 0x2c Img: 0x0 0xd8 1108.3303316634272
    177 Real:  0x7 0x2b Img: 0x0 0xd5 1109.1351603857765
    178 Real:  0x7 0x2a Img: 0x0 0xd7 1109.5925730447896
    179 Real:  0x7 0x2c Img: 0x0 0xd6 1108.469809280019
    180 Real:  0x7 0x27 Img: 0x0 0xd2 1111.7334731506105
    181 Real:  0x7 0x27 Img: 0x0 0xd6 1111.456025066772
    182 Real:  0x7 0x2b Img: 0x0 0xd8 1108.9260740832576
    183 Real:  0x7 0x29 Img: 0x0 0xe2 1109.3999777480442
    184 Real:  0x7 0x2a Img: 0x0 0xd6 1109.6623810670267
    185 Real:  0x7 0x29 Img: 0x0 0xdb 1109.906894365296
    186 Real:  0x7 0x29 Img: 0x0 0xda 1109.978064746254
    187 Real:  0x7 0x29 Img: 0x0 0xdd 1109.7636179672427
    188 Real:  0x7 0x27 Img: 0x0 0xd8 1111.3154172964132
    189 Real:  0x7 0x28 Img: 0x0 0xdb 1110.5042053941647
    190 Real:  0x7 0x29 Img: 0x0 0xd9 1110.0489230034777
    191 Real:  0x7 0x27 Img: 0x0 0xda 1111.17355564383
    192 Real:  0x7 0x2a Img: 0x0 0xdb 1109.3102209680608
    193 Real:  0x7 0x29 Img: 0x0 0xe0 1109.5463670557372
    194 Real:  0x7 0x26 Img: 0x0 0xde 1111.484316566753
    195 Real:  0x7 0x2d Img: 0x0 0xdd 1107.3816607579097
    196 Real:  0x7 0x2c Img: 0x0 0xdc 1108.0476456029046
    197 Real:  0x7 0x26 Img: 0x0 0xdd 1111.5567722812698
    198 Real:  0x7 0x2a Img: 0x0 0xe1 1108.8773530092242
    199 Real:  0x7 0x2e Img: 0x0 0xe0 1106.5722484864973
    200 Real:  0x7 0x2b Img: 0x0 0xdd 1108.5713691318772
    

    start:49k  add:10  num:200

    RFB:1000Ω

    J1 connect  1000Ω   and  1200Ω

  • Thanks for providing all this info and measurement results - all appears ok, except for the spikes. It begins to look like a real interference smothering your signal around 50 KHz. Do you have access to an oscilloscope to check whether the voltage at the AD5933 RFB pin (pin 4) is a well-formed, clean sine wave without any spikes and noise? Could the interference be coming from some pulse power supply? Your OPAMPs are supposed to be stable at unity gain, but it is still worth checking the voltage at both OPAMP's outputs to see if there may be some self-oscillation.

  • One more thing to check: are you using the Fre_To_Hex() function from the repository ad5933/User at master · edaworld/ad5933 (github.com) to calculate the Frequency Codes? For the AD5934 it should be
    dat = (2147483648 / (double)(AD5933_MCLK * 1000000)) * fre;
    Again, worth checking with the oscilloscope if the chip outputs the excitation frequency you programing in.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.