Post Go back to editing

AD6688采样单音信号时比较奇怪的现象

ADI的专家们你好,我在使用AD6688和ZCU102搭建数据采集系统。我的6688的采样率为2949.12MHz,采用了fs/4的NCO模式,使用第二奈奎斯特域采样,也就是3/4 * fs频率的2211.84MHz,当我给一个2211.84MHz的正弦信号时,我期待得到的是一条直线,因为频率被移动到了DC了。但是采集回来的数据却很奇怪,在一段时间会是固定的,但是另一端时间会有上升沿和下降沿,并且I路和Q路正好是反过来的,当I路读到的值为平台期(常值)时,Q路是上升沿或下降沿。反过来Q路值不变时,I路在上升沿或下降沿。上升到16390就不变了,下降到-16390也不变了,这两个值还出奇的对称。请问这是什么原因呢?我用其他频率的正弦波测试时是一切正常的。谢谢各位专家们的解答!