Post Go back to editing

ad9777

ad9777芯片手册的内插问题,对ad9777的寄存器进行配置,可以实现数据的四倍内插嘛?

Parents Reply
  • Hello initialdream666 , 

    What configuration are you using? CLKIN can function either as input data rate clock (PLL enabled) or as a DAC data rate clock (PLL disabled).

    1. If CLKIN is configured as input data rate then  DAC data rate clock =  input data rate * interpolation.
    2. If CLKIN is configured as DAC Data rate clock then   input data rate = DAC data rate clock  / Interpolation.

    In your example, I assume 25MHz is the data rate. the  DAC data rate clock would be multiplied by interpolation (4x) = 100MHz. Your 25MHz input data would be sampled by the 100MHz DAC clock. Please refer to page 27 - 32 of the datasheet for more details. Hope this helps.

    Kind Regards,

    Lorenz

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.