Post Go back to editing

AD2S1210的DOS失配如何消除

请教专家,读取故障寄存器值为0x10,无论如何调整SIN/COS值都无法消除故障,特来请教。目前我对各相关阈值寄存器配置如下:

1)DOS复位最大阈值寄存器(0x8b):0x7f;

2)DOS复位最小阈值(0x8c):0x01;

3)DOS超量程阈值(0x89):0x7f;

4)DOS失配阈值(0x8a):0x7f;

请帮忙解答两个问题:

1.对DOS失配阈值寄存器不是很理解,手册说是监控信号的最大值和最小值差值超过失配阈值即报失配故障,是指SIN±/COS±信号的幅值超过该阈值吗?我信号最大3.8V,最小1.2V,不论是最大最小还是幅值没有超过我配置的4.82V,所以不理解这个故障的原理;

2.如何能清除DOS失配故障,即故障寄存器(0xff)的"D4"位。