Post Go back to editing

About the data coherent synchronization of two channels in AD9174 dual link mode

Our requirement is that the phase difference of the waveforms output by the two channels in dual link mode is fixed, and this phase value is constant. But I found that when I changed the register configuration of AD9174, for example, only the gain was changed, the phase difference of the waveforms output by the two channels changed compared with before; so I would like to ask how to ensure the output of the two channels after changing the register configuration. Is the waveform phase difference the same as before?