Post Go back to editing

根据AD9680数字输出计算信号功率

大家好,我现在做了如下测试:信号源产生100M 12 dbm 的单音信号,连接到载板;载板上有一片AD9680;通过VIVADO  抓取到数字输出,现在要根据AD9680数字输出的计算出采集信号的功率是多少?我现在有几个疑问?

1/目前设置Vpp为1.7V,9680是14位ADC,数字输出8191是否对应1.7/2V?0.85V是否对应8192,还是对应其他大于4096的值?

2/现在采集到最大值为7800,是否能说明ADC输入的信号的峰值为1.7/8191*7800?

3/采集到的所有数字信号乘以1.7/8191(LSB)再做FFT,是否可以计算信号功率?

Parents Reply Children
No Data