Post Go back to editing

ad2s1210解码芯片报配置奇偶校验错误故障且位置信息突变

您好,目前使用贵司ad2s1210解码芯片,遇到上电偶尔报奇偶校验故障,且电机运行中存在位置信息突变情况。 位置和故障信息都是在配置模式通过spi读取,位置突变时都是D7位由0变为1,例如:电机不动时,旋变位置信息高8位为:00110110 偶尔突变到 10110110 。 目前生产打样了20块1210的板,其中10块出现上述异常现象,其他10台带电机运行一直未出现(已经连续工作了2个月)。 我们检查了上电时序和复位信号Vdd和RESET信号均满足规格书要求,报奇偶检验时通过示波器测量SDO信号,故障寄存器发出的数据D0位为1,确实是奇偶校验故障。 以上问题困扰了我们将近3周,实在没有其他头绪,若是有空,期待您的解惑... 谢谢!

Parents Reply Children
No Data