请问,需要输出40MHZ占空比50%的0-5V幅值调制信号,AD9704+运放的方式能否实现?

请问,需要输出40MHZ占空比50%的0-5V幅值调制信号,AD9704+运放的方式能否实现?

Hello,
Pls write the question in English, thanks!
AD9704 is one AC DAC @ max DAC rate fs=175Msps, the maximum bandwidth is fs/2, Firstly ,you should calculate the wanted signal bandwidth, if that is <fs/2, that is fine. BTW, you should put some margin on the bandwidth to ensure the construction filter to be easy built. if the DAC output level is not enough, op-amp can amplify the DAC output to your wanted level.
OK,we note that the AD9704 settling time is 11ns,Will it affect the bandwidth?