Post Go back to editing

AD5758使用问题

在使用AD5758时,按照收据手册中  PROGRAMMING SEQUENCE TO ENABLE THE OUTPUT  描述的步骤来配置AD5758;

等配置好后,AD5758的VIOUT引脚有输出,但输出不能通过指令操控。如果操作寄存器6配置成电压模式

0010: ±5 V voltage range. 输出时,则输出-4.9V的固定电压,如果配置成 1100: ±24 mA current range 电流输出时,则输出固定23.9ma的电流。

我操作DAC Input Register 寄存器 ,并使用LDAC更新指令,VIOUT脚输出没有变化,而后我读取 DAC output register,发现数据确实更新了,但是输出端口没有变化。

请问这是什么原因?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.