Post Go back to editing

AD5421输出4mA电流偏差的问题

应用于HART仪表,使用了AD5421+AD5700套片来实现HART通信,我们自己绘制并焊接了一些开发板,开发板上除了HART套片外还有一个MSP432单片机以及一些放大器。
在实际使用中发现当设定输出4mA时,部分开发板输出为4.6mA、部分开发板一开始输出为4mA随后逐渐变化为4.6mA、部分开发板可以输出4mA。
AD5421使用了4-20mA工作模式,尝试调整了失调寄存器等参数对其没有影响。
开发板上因功耗问题,AD5421输出12V电压,使用了一个LTC3388 DCDC转换器为全板提供3.3V供电,当AD5421设置为最小电流模式时大约为1.2mA电流。
电流的测试方法使用一个串联在24V环路中的10欧姆检流电阻测出。

希望能获得一些帮助

Parents Reply Children