------------------------------------------------
------------------------------------------------
HELLO, does it work with you or are there any cons
Hi,
You can refer to the existing AD7768-1 mbed example project.
Mbed supports a variety of stm32 boards.
Regards,
Pratyush
Hi Pratyush,
thank you for the answer
Yes it is good solution thank you, but the problem mbed forced special card like SDP-K1 and forced the use of intefece mbed. and me I wished to study stm32cubeide, I found some solution with which I can etulisé intreption or DMA to read the data of the ADC put I believe very complicated.
Benjdida,
Hi Benjdida ,
Mbed enables our firmware to support any supported mbed enabled board (~170 total, 55 are STM32 of them currently). Here is a list of boards that mbed supports:
Development boards | Mbed
Even our existing firmware, with the help of no-OS drivers, can be ported to the STM32 platform or any platform with little modifications. You can refer to this page for more information: Understanding and Using the No-OS and Platform Drivers | Analog Devices
Regards,
Pratyush
Hi Pratyush,
I will try to work on this solution. .
Benjdida,