我用AD7684搭建了一款AD转换电路,我把输入(IN+和IN-)短路,共同连接到参考电源上(4V),读出来的数据为0x533而不是"0",再把输入短路后,重新共同连接到Ref/2的偏置电压上,读出来的值约为0x34,也就是说共模误差抑制好差,这是什么原因?我想AD7684原厂样品不会有问题吧,可是我也看不出电路上有什么问题,所以来请大家指教!谢谢!
我用AD7684搭建了一款AD转换电路,我把输入(IN+和IN-)短路,共同连接到参考电源上(4V),读出来的数据为0x533而不是"0",再把输入短路后,重新共同连接到Ref/2的偏置电压上,读出来的值约为0x34,也就是说共模误差抑制好差,这是什么原因?我想AD7684原厂样品不会有问题吧,可是我也看不出电路上有什么问题,所以来请大家指教!谢谢!
因为Common-Mode Input Range +IN, −IN: min.0; typ. VREF/2; max. VREF/2 + 0.1 V
非常感谢StevenX的指导,我今天早晨又去看了一下,是这个问题,我平时设置的共模电压是2.5V,Vref=4V.超过了Vref/2+01V的高大值,所以会出上述问题,问题已经解决,不知道怎么感谢!