CN0326 - pH Moniter with AD7793

您好,关于CN0326电路笔记中对AD7793信号输入的处理方式,我有几点不明白:

1、“ADC采用单电源供电,采用外部基准电压源1.05V,增益配置为1,满量程输入输入范围为±Vref=±1.05V”,这句话是否说明了AD7793的模拟输入通道可以直接输入低于0V的电压信号并直接转换,比如输入-0.5V?

2、“AIN1+端输入双极性信号,ADC单电源供电,所以输入信号应偏置到地以上,偏置电压的产生方式是在AIN1-端输入1.05V共模偏置电压”,能否具体讲解一下偏置电压配置的原理?AIN1-端输入1.05V共模偏置电压后,AIN1+端的输入信号范围是多少呢?如果差分输入的一端需要输入双极性信号(ADC单电源供电,基准电压也是单极性),那么差分输入的另一端应该怎样处理?

期待您的回复。

请参见下图:

Parents Reply Children
No Data