Post Go back to editing

AD7760的运放差分输入(VinA+/VinA-)共模电压范围

AD7760 datasheet里似乎没有明确的说明内置运放输入(VinA+/VinA-)的允许共模电压范围,图52的例子里给的是共模电压0V,输入±2.5V的信号。

如果我希望在VinA+/VinA-输入2.5±2V的差分信号,共模电压是2.5V是否可以?(AVdd3=5V)

另外手册Absolute maximum rating里给出的参数VINA+, VINA− to GND1 是 −0.3 V to +6 V,这是不是和图52里 VINA+/VINA-输入0±2.5V有矛盾?

谢谢!