现在用FPGA并行总线读取AD7616数据,配置硬件突发模式,一次转换16通道,量程±5V,采用内部电压基准。模拟端输入电阻匹配1K,电容0.1uF。模拟输入端VxxGND接地了。当在VA1端加5V电压时,转换结果为26503,找一系列电压点进行测试,结果如下。
1.2V转换结果2146,
1.8V转换结果5653,
2.5V转换结果10229,
3.3V转换结果15372,
悬浮的引脚,结果为5054,。并且用万用表测量,悬浮引脚有1.5V的电压。现在不知道该怎么查找问题。第一次发帖,不知道怎么插入图片,硬件原理图和FPGA读取结果图没有放上。