请教AD9914产生100MHz-600MHz锯齿波扫频源(数字斜坡扫频)

       我做了一个AD9914的信号产生板,近一个月用AD9914的Digital Ramp Modulation(linear sweep)模式产生100MHz-600MHz的锯齿波扫频信号时,总产生不了。(ps:这个板子使用Profile M​odulation产生了100MHz-1GHz的跳频源,因此可以排除板子硬件设计问题) ​

       我是使用100MHz外部晶振,通过AD9914内部PLL倍频25倍到2.5GHz。关于​使用Digital Ramp Modulation(linear sweep)模式,产生100MHz-600MHz的锯齿波扫频信号,我有以下3个问题请教一下:

       1、是否需要配置外部引脚​Pi​n2​5、26、27[PS0、PS1、PS2],换句话说是否需要配置单频寄存器Profile 0?​

       2、外部引脚上:①使用SPI串行通信方式,配置了F[3:0]为[0,0,0,1]. ②控制板连上AD9914引脚Pin22​​、21、20、85、67、86(即: CS、SCLK、SDIO、Master_Reset、EXT_PWR_DWN、I/O_UPDATE)​ ​③​引脚Pin63[DRCTL]设置为高电平(因为需要产生锯齿波,因此是正斜率信号输出)​④引脚Pin64[DRHOLD]设置为低电平(正常扫描)。请问外部引脚配置正确吗?还需要配置其他外部引脚吗?​

       3、寄存器配置上:​​ CFR1(0x01,0x03,0x00,0x00)、​CFR2(0x00,0x0C,0x28,0x00)、CFR3(0x00,0x44,0x11,0x50)、Digital Ramp Lower Limit Register(0x0A,0x3D,0x70,0xA4)、 Digital Ramp Upper Limit Register(0x3D,0x70,0xA3,0xD7)、Rising Digital Ramp Step Size Register(0x00,0x5E,0x5F,0x31)、Digital Ramp Rate Register(0x00,0x00,0x00,0x0F).请问寄存器配置正确吗?

       谢谢帮忙!Best Wishes!