CN0287可以SPI级联使用嘛

我在CN0287的板子上测试,并没有用到ADT7310,片选没有设置,为什么会出现一个3.3V左右的高电压,而且,我自己做了一个长板子,24通道,6路,每路都是分开的,打算用GPIO模拟SPI,因为片选是分开的,我觉得这样可以级联使用,但是DOUT在保持一段高电平后就变低了,在CN0287上,同样的程序,看到的是DOUT一直保持高电平,经过自己的检查,把ADT7310焊下去波形就和我自己的板子波形一样了,不是很理解,因为我并没有用到ADT7310

Parents
  • 底下的评论框出不来,我就在这里回复一下把,我现在是在WIN上用STM32IDE写的程序,然后GPIO模拟SPI,单路的话,AD7193和AD738的片选都设置了,ADT7310的片选没有设置,,现在做的新板子我去掉了ADT7310这一块,然后同一组SPI接口,多个片选接口,调试过能做到两路数据输出,第三路就不可以了,如何保证程序相同,因为我烧写的是同一组程序

Reply
  • 底下的评论框出不来,我就在这里回复一下把,我现在是在WIN上用STM32IDE写的程序,然后GPIO模拟SPI,单路的话,AD7193和AD738的片选都设置了,ADT7310的片选没有设置,,现在做的新板子我去掉了ADT7310这一块,然后同一组SPI接口,多个片选接口,调试过能做到两路数据输出,第三路就不可以了,如何保证程序相同,因为我烧写的是同一组程序

Children
No Data