stm32使用spi读取外部ADC(LTC2500-32)数据问题

本人因设计需求要使用stm32读取ltc2500-32的ADC数据,该款芯片有两种模式(32位数字滤波输出和24位差分+7位共模+1位溢出位输出),现在设计需要24位的输出,但在使用spi与之通信时遇到问题.spi通信需要MISO和MOSI,但是在使用24bit功能时,只有SDO和SCK引脚,另外的RDLB拉低即可,没有片选信号接入,BUSY信号也是由ADC芯片输出的,这时SPI通信该怎么配置呢?

因为要去读32位数据在再进行移位操作,这样写可以工作吗?还有stm32的MOSI引脚和片选该怎么去接线,ADC芯片上的SDI引脚只对A模式(32位模式)起作用,请问是吗?