Post Go back to editing

关于AD7989-1BRMZ采样不准确

1/设计电路如图,驱动采用AD8476BRMZ,2.5V基准使用ADR4525BRZ,基准电压测试稳定,

2/在测试过程中,ADB476BRMZ输入电压10mV,但是AD采样电压得到会有10几mV,测量偏差非常大。

3/通过整改,删除差分输入的RC滤波,ADB476BRMZ输入电压10mV,差分输入电压比较稳定的10.1mV,电压稳定,但是AD采样电压得到会有11mV,多次测试不稳定偏差大概±1mV

  • 1. AD7989-1共模输入范围为VREF × 0.475《VREF × 0.5《 VREF × 0.525, 建议AD8476的VOCM接到VREFx0.5的电平上。

    2. AD7989-1前的RC不要去掉。

    3. AD7989-1参考引脚去耦电容应该为10uF. Reference Input Voltage. The REF range is 2.4 V to 5.1 V. This pin is referred to the GND pin and must be decoupled closely to the GND pin with a 10 μF capacitor.

    4. 如果还不行,可以给ADR4525输出加个buffer, 比如ADA4805来驱动ADC参考输入引脚。