Post Go back to editing

LTC2410

请问:

    我用LTC2410单端输入,IN-接地,REF-接地,REF+接MAX6126 2.5V基准,CS,SCLK,SDO三线输入,IN+直接连到运放的输出端。刚开始发现问题是由于测量值不准,100。00MV电压测量结果只有98.30MV,用示波器看IN+端波形发现有干扰,将IN+和运放断开,运放输出端只有UV级别噪声,IN+通过10K电阻接地,发现它上面在CS由低电平变为高电平,也就是读取数据结束后,有大约100MS长度的高频信号,峰值幅度超过500MV,将IN+通过300欧姆电阻和运放输出端连接,并联一个2UF陶瓷电容到地,测量值最后在100.00MV附近跳动,跳动约0.06MV,用万用表测量IN+端电压也有波动,但是将IN+和运放之间的电阻断开,运放的输出是稳定的,也就是IN+脚自身产生了干扰,请问这种情况是LTC2410损坏了,还是其他什么原因?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.