Post Go back to editing

AD7606测量结果为实际值的4 - 4.5倍

        首先,我在前一块板子上做实验的时候因为没有去耦,导致CONVSTX信号有干扰而致使采样频率很靠近250K,但是采样得到的数据都是正确的,所以我认为编码转换上我应该是没有问题的。

        后来我修改了板子,这次没有干扰了,采样频率50K,没有过采样,8个通道实际使用4个,通过示波器观察应该都没有问题。

        然后进行测量,结果发现测量的正值总是实际值的4.5倍左右,负值总是实际值的4倍左右。

        比如我测一个50Hz的0.2Vpp+0.2Vdc的方波,结果低电平是0.47V,高电平是1.34V;测0.2Vpp-0.6Vdc的方波,结果低电平是-2.89V,高电平是-2.02V。我测了很多组都差不多这样,但是频率都是对的,是50HZ整。我是用FPGA控制的,串口通信。

        我找了半天也想不出原因,不知道是不是电路设计上又有问题,希望得到建议,谢谢。贴片电阻我用的都是100欧的。