Post Go back to editing

IF sampling frequencies vs FPBW

On the first page of AD9265 datasheet, it mentions that "IF sampling frequencies to 300 MHz" and "Differential analog inputs with 650 MHz bandwidth”.  I think 650MHz is the 3dB full power BW, then we can input analog signal up to 650MHz. Right? How to understand "IF sampling frequencies to 300 MHz"? What's its meaning?

Top Replies

  • FormerMember
    FormerMember
Aug 21, 2019 +1 verified

Hello,

Your understanding of the BW is correct and one could inject signals up to (and beyond) 650 MHz if the loss (3dB+) and performance degradation is considered acceptable for the application.  IF sampling…