张力传感器信号转换芯片推荐!

目前要做一个张力信号放大器,需要采集两路±200mV和±20mV的差分信号,经过放大后输出0-10V和4-20mA的信号,在网上找到好像有很多芯片可以实现,但不知道哪款更合适,如AD7730,AD7792和AD7798等。


  • The characteristics of the sensor include   www.allicdata.com/list.html : miniaturization, digitization, intelligence, multi-functionality, systemization, and networking. It not only promotes the transformation and upgrading of traditional industries , but also may establish new industries, thus becoming a new economic growth in the 21st century. point. Miniaturization is based on microelectromechanical systems (MEMS) technology and has been successfully applied to silicon devices as silicon pressure sensors.