ltc2107 or ltc2185 SPI program

HI

   当用SPI配置LTC2017或者LTC2108的时候需要注意什么?

   因为我用fpga配置以上两个芯片,总是不能成功,而相同的主程序,配置ad9520,ad9510,ad9858等都可以。这些程序里面我只修改了相关的寄存器数量和相关寄存器内容,以下是寄存器的内容:

assign data95[0]=16'b0000_0000_0000_0000;
assign data95[1]=16'b0000_0000_1000_0000;
assign data95[2]=16'b0000_0001_0000_0000;
assign data95[3]=16'b0000_0010_0000_0000;
assign data95[4]=16'b0000_0011_0000_1001;
assign data95[5]=16'b0000_0100_0010_1000;
assign data95[6]=16'b0000_0101_0000_0001;

另外,fpga用的是kc705的开发板,接口应该是2.5V的

谢谢!