AD5560供电电压和输出级电压的关系

你好,选择外部大电流范围手册说可以输出到AVDD-2.25V的高压,请问这个电流能力是多少?

在实际测量中发现:选择外部1.2A的电流量程输出高压小电流时,芯片的HCAVDD1管脚的电压竟然和输出电压一样,这是为什么?

假如AVDD=25V,HCAVDD1=6.5V,AVSS=HCAVSS1=-5V:

在1.2A的量程下:芯片Force一个2V,1mA的输出,这个2V是来自AVDD还是HCAVDD1?继续增大2V使得其变成10V,1mA,请问芯片内部在哪一点开始切换供电电压轨,芯片切换的机制是什么?

多谢!



为什么问题都10多天还没有回复?是哪里描述不清晰吗?
[edited by: Shawn_Tao at 2:59 AM (GMT 0) on 11 Mar 2019]