Post Go back to editing

AD8138+AD9244+AD6620的结构如何替换?

因为AD6620已不做推荐,AD8138+AD9244+AD6620的结构形式应该如何替换?

  • Hi, 

    The AD9244 + AD6620 function are integrated together in some of our latest converter products, for example the AD9695.  In general you do not see stand alone digital down converters and filters as stand alone products (like the AD6620), they are either integrated into the converter or are implemented in an FPGA or digital ASIC.  If the AD8138 was simply a buffer, then again products like the AD9695 include an integrated buffer.  If you were using it for gain, you would still need to pick an appropriate amplifier to replace that block.  

    ADI also offers very highly integrated transceivers, like the AD9361 that can provide a higher level system solution.  

    Regards, 

    David

  • 竟然收到了回复,内心十分激动!Thank you very much,very much,very much.

  • AD6620的设计软件Fltdsgn.exe你有吗?哪里可以下载到

  • Hi, 

    No, unfortunately, this software was discontinued many years ago and the product was classified as "Not recommended for new designs".  We still support existing designs but do not have evaluation or design tools to support new designs.  I would recommend considering an ADC product that integrates these features into a single chip for your new design.   The AD9695 might be a good one to consider

    Regards, 

    David