我使用AD7711ARZ这款ADC作为温度采集调理时候,为了节约PCB设计空间,时钟电路电路部分采用的无源10MHz的晶体(该晶体参数:负载电容为Cl=20pF,振荡模式:AT基频,串联谐振电阻最大Rr=50Ω,频率稳定度:±30PPM,工作温度范围为-40℃~85℃,激励功率最大0.1mW)由于采用的无源晶体我设计时候加了两个22pF的对地负载电容,实际使用的过程中发现常温25℃晶体起振很慢,起振时间有些达到200mS,在低温接近0℃及以下会出现晶体不起振或者器振更长,导致软件无法正常配置控制AD7711寄存器。当在常温或者低温下去掉两个负载22pF的负载电容,晶体起振时间减小到60mS左右,但起振时间还是明显超出晶体的本身的1mS的起振指标,为了排除晶体的问题,把这些晶体拿回厂家做过对比试验及全温度范围温度试验,该晶体技术指标都指标之内,起振时间及性能良好(1mS起振时间),高低温参数没有发生明显改变。已经核实测试过AD7711电源供电良好,采用LDO-TPS76350供电,能满足全温度范围,电压在5V±1%,上电时间760uS,噪声非常小。PCB布局良好,晶体走线分布电容理论上小于0.5pF,通过反复测试现在找不到该问题的原因所致,我看到官方的AD7711运用手册AN-366上也取消了无源晶体外接负载电容,AD7711在这个无源晶体使用上有什么特殊之处吗,请ADI工程师帮我分析下,给些解决的办法,谢谢了!